I am trying to connect a custom board (based on the schematics of EVM5505) with TMS320C5505 with an XDS100v1 emulator.
After starting CCSv4.1.1 , while trying to connect to the target board , i get the following error:
"Error connecting to the target:(Error -1063 @ 0x0)Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver.(Release 5.0.333.0)"
The same emulator works fine with a different EVM5505 , manufactured by Spectrum Digital with an onboard TMS320VC5505, so the drivers for the XDS100v1 emulator are definitely working fine.
1. The error message is written above.
2. CCS version is 4.1.1.
3. CCS Installation directiory is C:\ccs4
4. .ccxml file found in "C:\Users\Abhishek\Desktop\Targetconfig\Newtargetconfiguration.ccxml"
5. I am using the evm5505.gel file, found in the documentation of spectrum digital. http://support.spectrumdigital.com/boards/evm5505/revd/
6. Emulator used XDS100v1
7. It is a custom board designed with reference to EVM5505. The difference being that the EVM5505 used for prototyping had a VC5505 , while the custom board has a C5505. Appropriate changes have been made accordingly in the hardware based on documentation on migration from VC5505 to C5505.
8. Target connector is a 14 pin JTAG.
9. Please find below schematic snapshot of JTAG connections, the pins are connected to appropriate pins of C5505.

10. Host operating system : Windows 7, 64 bit
11. A JTAG diagnostic was run using the dbgjtag.exe GUI. All tests viz. Scan Path Length, Broken Path and Integrity test passed successfully. please find log below.
12. I am using the on chip RTC oscillator, and SPI(Atmel25256) and I2C EEPROMs(24W256) for memory.
Since, the dbgjtag diagnostics went fine,it makes me think that the hardware is probably fine. Is the problem the gel and pll settings, maybe the difference is that the EVM5505 with which the emulator works fine has a VC5505 on board, where as our custom board has a C5505? If yes, can i get the appropriate gel file ?
Please correct me if i am wrong!
A quick response would be VERY helpful, as i am on a deadline!
Thanks Abhishek
Log of dbgjtag test:
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Feb 28 2011'.
The library build time was '22:16:13'.
The library package version is '5.0.333.0'.
The library component version is '35.34.29.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will now attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Feb 28 2011'.
The library build time was '22:16:13'.
The library package version is '5.0.333.0'.
The library component version is '35.34.29.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will now attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[Perform the standard path-length test on the JTAG IR and DR]-----------
This path-length test uses blocks of 512 32-bit words.
|| // -- \\ The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 38 bits.
The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Feb 28 2011'.
The library build time was '22:16:13'.
The library package version is '5.0.333.0'.
The library component version is '35.34.29.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will now attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[Perform the Broken Path scan-test on the JTAG IR]----------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Broken Path scan-test has succeeded.
-----[Perform the Broken Path scan-test on the JTAG DR]----------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Broken Path scan-test has succeeded.
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Feb 28 2011'.
The library build time was '22:16:13'.
The library package version is '5.0.333.0'.
The library component version is '35.34.29.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will now attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[Perform the Given Data scan-test on the JTAG IR]-----------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
It uses the first 1 of the 10 different test-cases.
Do a test using 0x5533CCAA.
Scan tests: 1, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Given Data scan-test has succeeded.
-----[Perform the Given Data scan-test on the JTAG DR]-----------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
It uses the first 1 of the 10 different test-cases.
Do a test using 0x5533CCAA.
Scan tests: 1, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Given Data scan-test has succeeded.