Other Parts Discussed in Thread: TMS320VC5505
Hi,
can anybody tell me what CCS4 or the JTAG does exactly in addition to the commands defined in the GEL file when "Connect", "Run" and "Halt" from the Target menu are selected?
My program seems to work from EEPROM properly only after a Connect-Run-Halt-Run sequence (no load, of course). The code basically executes from EEPROM on power-up without CCS4, but the DMA doesn't work, the interrupts are never triggered. After the sequence described it works completely. This is not due to the GEL commands, I commented them completely out and the behaviour stays the same. Any suggestions?
Regards,
Raphael