Other Parts Discussed in Thread: TMS320C5515
Hi, I have a Spectrum Digital TMS320C5515 ezDSP on which I want to use timer interrupts using DSP/BIOS. However, my interrupt function is never called, even though the timer interrupt flags in IFR0 and TIAFR are set. My Code is attached. The timer part in the tcf file: bios.CLK.TIMER1FUNC = prog.extern("f"); bios.CLK.TIMERSELECT = "Timer 1"; bios.CLK.CONFIGURETIMER = 0; Thanks in advance