This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Activating NAND on TI TNETV1051 EVB (aries)



Hi,

I am using TI TNETV1051 EVB.

I've connected NAND to CS0 (using jumpers) and set SW2 to NAND.

I do see that with pspboot I am able to use NAND (able to use NBL), however when i try to load the kernel, i get a kernel panic.

I tracked the kernel panic to do_map_probe in avalanche_flash_init.

I am using Linux 2.6.10, and changed the following configuration in config files:

CONFIG_MTD_AVALANCHE_CHIP0_START=0x10000000

CONFIG_MTD_NAND_AVALANCHE_CS=0

However still get same kernel panic since i faile to successfully probe NAND mtd.

I searched documentation but couldn't find any usefull data.

Can you please assit?

Thanks,

Idan.

  • Hi Idan
    This forum is primarily for c5000 device family.
    We don't have anyone on the team monitoring this forum that is knowledgeable about the TNET family devices.
    Regards
    Mukul
  • Hi Mukul,

    Thank you for the quick response.

    I posted in this forum since i saw that also previous question about TNETV were posted here.
    Can you please refer me to a forum that does support TNETV1051?

    Thanks,
    Idan.
  • Hi Idan
    Yes we have had few questions here that we have previously tried to address to the best of our ability, but again this is not the forum for those devices. This is an old device and not too much prevalent in broad market, so there is no dedicated forum for support of this device.

    I have forwarded this thread to the business unit that owns the legacy support for this device, to see if they can provide any guidance on where you can route these questions. I will update this post, if I hear back something from them.
    Sorry for not being much help on this.
    Regards
    Mukul
  • Hi Idan,

    Are you working with any local TI field engineer? There is separate dedicated support model for TNET devices. Can you ask TI field engineer to get in touch with me at bkharadi@ti.com ? I can provide the support structure where this question can be posted.

    Regards,
    Bhavin