Part Number: TMS320C5505
Dear ,
following is my code..
i want read adc channel after every 1ms delay.
i followed TI's timer guideline and sample code too...
but i am not getting exact 1ms..it hits after every 400ms not 1ms..kindly go through it and tell me what an issue.
#include <stdio.h>
#include "csl_gpt.h"
#include "csl_intc.h"
#include <csl_general.h>
#include "csl_uart.h"
#include "csl_uartAux.h"
#include "csl_sysctrl.h"
#include "usbstk5515.h"
#include "usbstk5515_uart.h"
#include "usbstk5515_gpio.h"
#include "usbstk5515_led.h"
#define SARCTRL ((ioport volatile unsigned*)0x7012)
#define SARDATA ((ioport volatile unsigned*)0x7014)
#define SARCLKCTRL ((ioport volatile unsigned*)0x7016)
#define SARPINCTRL ((ioport volatile unsigned*)0x7018)
#define SARGPOCTRL ((ioport volatile unsigned*)0x701A)
#define SYS_PCGCR1 *(volatile ioport Uint16*)(0x1c02)
#define SYS_PCGCR2 *(volatile ioport Uint16*)(0x1c03)
#define WR_STR_LEN (80u)
#define RD_STR_LEN (10u)
#define CSL_PLL_DIV_000 (0)
#define CSL_PLL_DIV_001 (1u)
#define CSL_PLL_DIV_002 (2u)
#define CSL_PLL_DIV_003 (3u)
#define CSL_PLL_DIV_004 (4u)
#define CSL_PLL_DIV_005 (5u)
#define CSL_PLL_DIV_006 (6u)
#define CSL_PLL_DIV_007 (7u)
#define CSL_PLL_CLOCKIN (32768u)
#define PLL_CNTL1 *(ioport volatile unsigned *)0x1C20
#define PLL_CNTL2 *(ioport volatile unsigned *)0x1C21
#define PLL_CNTL3 *(ioport volatile unsigned *)0x1C22
#define PLL_CNTL4 *(ioport volatile unsigned *)0x1C23
#define CSL_TEST_FAILED (1u)
#define CSL_TEST_PASSED (0)
extern void VECSTART(void);
Uint32 cpuCycleCount = 0;
Uint32 sysClk;
volatile Uint16 hitIsr = 0;
int adc_out[65]=0,Tx_data_lsb,Tx_data_msb,i=0,j,count=0,count_int;
int ADC_data[1300];
int adc_single_data=0;
char *str={"\n ADC data :"};
char msg[]={" "};
char msg1='s';
char *wrbuffer;
char *result;
CSL_Handle hGpt;
Int32 Read_GPAIN1(void);
void Init_SAR(void);
Int16 EVM5515_UART_open( );
Int16 CSL_gptIntrTest(void);
Uint32 getSysClk(void);
void Send_data(int adc_data);
/**
* \brief GPT Interrupt Service Routine
*
* \param none
*
* \return none
*/
interrupt void gpt0Isr(void)
{
hitIsr = TRUE;
/* Clear Timer Interrupt Aggregation Flag Register (TIAFR) */
CSL_SYSCTRL_REGS->TIAFR = 0x01;
//USBSTK5515_ULED_on(4);
USBSTK5515_ULED_off(3);
USBSTK5515_waitusec(1000);
USBSTK5515_ULED_on(3);
USBSTK5515_waitusec(1000);
/*for(i=0;msg[i]!='\0';i++)
{
while((UART_LSR & 0x60)==0); // Wait for TX ready
EVM5515_UART_putChar(msg[i]); // Write 1 byte
}*/
//Send_data(adc_single_data);
for(i=0;i<100;i++)
{
adc_out[i]=Read_GPAIN1();
}
// Send_data(adc_out[i]);
count_int++;
printf("\nvalue of count= %d\n",count_int);
IRQ_clear(TINT_EVENT);
}
void main(void)
{
int i=0;
SYS_PCGCR1=0; //INIT clock
SYS_PCGCR2=0; //INIT clock
SYS_EXBUSSEL = 0x0A00; // Enable user LEDs on external bus
//USBSTK5515_GPIO_setDirection( 18, GPIO_OUT );
USBSTK5515_ULED_init();
EVM5515_UART_open();
printf("\nadc testing");
Init_SAR();
/*for(j=0;j<20;j++)
{
CSL_gptIntrTest();
}
while(i!=1240)
{
ADC_data[i]=adc_out[i];
i++;
}*/
while(1)
{
// printf("the value of i= %d",i);
CSL_gptIntrTest();
}
}
void Send_data(int adc_data)
{
Tx_data_lsb=(adc_data&0xFF); //lsb
Tx_data_msb=((adc_data>>8)&0xFF);//msb
while((UART_LSR & 0x60)==0); // Wait for TX ready
EVM5515_UART_putChar(Tx_data_lsb); // Write 1 byte
USBSTK5515_waitusec(1000);
EVM5515_UART_putChar(Tx_data_msb); // Write 1 byte
USBSTK5515_waitusec(1000);
}
void Init_SAR(void)
{
//*SARCTRL = 0x4000; //select ch4, GPAIN2
*SARCTRL = 0x3400; // Select AIN3, which is GPAIN1
*SARCLKCTRL = 0x0031; // 100/50 = 2MHz
*SARPINCTRL = 0x7104; //Bandgap-Based Reference Voltage set to 0.8V.
*SARGPOCTRL = 0;
return;
}
Int32 Read_GPAIN1(void)
{
Int32 val=0;
Uint16 i;
//bit15=soc,bit 14 13 12 i.e 011 so ch3 is selected,bit 10=1 for only one conversion.
// *SARCTRL = 0xB400; //for ch3 single conv
*SARCTRL = 0xB800; //for ch3 continuous conv
// *SARCTRL = 0xC000; //ch4 continuous conv
while(1)
{
for(i=0;i<50; i++)
asm(" nop");
val = *SARDATA;
//val=(val/1023);
if((val&0x8000) == 0)
{
break;
}
}
return val;
}
Int16 CSL_gptIntrTest(void)
{
CSL_Status status;
CSL_Config hwConfig;
CSL_GptObj gptObj;
Uint32 cpuCycleDelta;
hitIsr = FALSE;
status = 0;
/* Get the System clock value at which CPU is currently running */
sysClk = getSysClk();
/* CPU clock cycles that are 1% of the sysClk" value */
cpuCycleDelta = (sysClk/100);
printf("\n\nCPU clock is running at %ldKHz\n", sysClk);
printf("Timer Prescaler Divide Value is Set to Divide by 4\n");
printf("GPT Runs at Rate 1/4 of the CPU System Clock\n");
printf("GPT Count is Initialized to 1/4 of CPU Clock Cycles per Millisecond\n");
printf("With Reference to CPU Clock GPT Will Take 1 Millisecond to Count Down the Timer to 0\n");
printf("So The CPU Should Execute Approximately %ld(±1%%) Clock Cycles ",sysClk);
printf("From the Starting of the Timer Till the Expiry of the Timer\n\n");
/* Open the CSL GPT module */
hGpt = GPT_open (GPT_0, &gptObj, &status);
if((NULL == hGpt) || (CSL_SOK != status))
{
printf("GPT Open Failed\n");
return (CSL_TEST_FAILED);
}
else
{
printf("GPT Open Successful\n");
}
/* Reset the GPT module */
status = GPT_reset(hGpt);
if(CSL_SOK != status)
{
printf("GPT Reset Failed\n");
return (CSL_TEST_FAILED);
}
else
{
printf("GPT Reset Successful\n");
}
/* Clear any pending interrupts */
IRQ_clearAll();
/* Disable all the interrupts */
IRQ_disableAll();
IRQ_setVecs((Uint32)(&VECSTART));
IRQ_plug(TINT_EVENT, &gpt0Isr);
IRQ_enable(TINT_EVENT);
hwConfig.autoLoad = GPT_AUTO_ENABLE;
hwConfig.ctrlTim = GPT_TIMER_ENABLE;
hwConfig.preScaleDiv = GPT_PRE_SC_DIV_1;
//for 1ms
// hwConfig.prdLow = (sysClk)/4;
//hwConfig.prdHigh = 0x0000;
hwConfig.prdLow = (((sysClk)*5)&0xFFFF);
hwConfig.prdHigh = (((sysClk)*5)>>16);
//for 20ms 5*sysclk=5*262000=1310000=13FD30
//for 1000ms=1sec=250*sysclk=250*262000=65500000=03E77360
//hwConfig.prdLow = 0x7360;
//hwConfig.prdHigh = 0x03E7;
/* Configure the GPT module */
status = GPT_config(hGpt, &hwConfig);
if(CSL_SOK != status)
{
printf("GPT Config Failed\n");
return (CSL_TEST_FAILED);
}
else
{
printf("GPT Config Successful\n");
}
/* Enable CPU Interrupts */
IRQ_globalEnable();
/* Start the Timer */
GPT_start(hGpt);
/* Wait for the timer interrupt */
/* This loop takes 12 CPU cycles to execute on iteration.
So the CPU cycles executed after starting the timer till the
expiry of the timer will be 12*cpuCycleCount. */
while(hitIsr != TRUE)
{
cpuCycleCount++;
}
/* Disable the CPU interrupts */
IRQ_globalDisable();
/* Clear any pending interrupts */
IRQ_clearAll();
/* Disable all the interrupts */
IRQ_disableAll();
/* Stop the Timer */
status = GPT_stop(hGpt);
if(CSL_SOK != status)
{
printf("GPT Stop Failed \n");
return (CSL_TEST_FAILED);
}
else
{
printf("GPT Stop Successful\n");
}
status = GPT_reset(hGpt);
/* Display the number of CPU cycles executed */
printf("\nTimer Count Reached Zero\n");
cpuCycleCount *= 12;
printf("\n\nNUMBER OF CPU CYCLES EXECUTED AFTER STARTING THE TIMER TILL THE TIMER EXPIRY: ");
printf("%ld\n", cpuCycleCount);
/* Test passes if the "cpuCycles" value is in the range
((sysClk) ± (1% of sysClk)) */
if(((cpuCycleCount - cpuCycleDelta) < sysClk) &&
((cpuCycleCount + cpuCycleDelta) > sysClk))
{
printf("GPT IS RUNNING AT THE CONFIGURED RATE!\n\n");
}
else
{
printf("GPT IS NOT RUNNING AT THE CONFIGURED RATE!\n\n");
return (CSL_TEST_FAILED);
}
/* Close The GPT Module */
status = GPT_close(hGpt);
if(CSL_SOK != status)
{
printf("GPT Close Failed\n");
return (CSL_TEST_FAILED);
}
return (CSL_TEST_PASSED);
}
#if (defined(CHIP_C5505_C5515) || defined(CHIP_C5504_C5514))
Uint32 getSysClk(void)
{
Bool pllRDBypass;
Bool pllOutDiv;
Uint32 sysClk;
Uint16 pllM;
Uint16 pllRD;
Uint16 pllOD;
pllM = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR1, SYS_CGCR1_M);
pllRD = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDRATIO);
pllOD = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_ODRATIO);
pllRDBypass = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDBYPASS);
pllOutDiv = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_OUTDIVEN);
sysClk = CSL_PLL_CLOCKIN;
if (0 == pllRDBypass)
{
sysClk = sysClk/(pllRD + 4);
}
sysClk = (sysClk * (pllM + 4));
if (1 == pllOutDiv)
{
sysClk = sysClk/(pllOD + 1);
}
/* Return the value of system clock in KHz */
return(sysClk/1000);
}
#elif (defined(CHIP_C5517))
Uint32 getSysClk(void)
{
Uint32 sysClk;
float Multiplier;
Uint16 OD;
Uint16 OD2;
Uint16 RD, RefClk;
Uint32 temp1, temp2, temp3, vco;
Uint16 DIV;
temp2 = PLL_CNTL2;
temp3 = (temp2 & 0x8000) <<1 ;
temp1 = temp3 + PLL_CNTL1;
Multiplier = temp1/256 +1;
RD = (PLL_CNTL2 & 0x003F) ;
RefClk = 12000/(RD+1);
vco = Multiplier * (Uint32)RefClk;
OD = (PLL_CNTL4 & 0x7);
sysClk = vco/(OD+1);
OD2 = ((PLL_CNTL4 >> 10) & 0x1F) ;
if (PLL_CNTL3 & 0x8000) // PLL Bypass
sysClk = RefClk;
else
sysClk = vco/(OD+1);
if ((PLL_CNTL4 & 0x0020) == 0) /* OutDiv2 */
sysClk = sysClk / ( 2*(OD2+1));
/* Return the value of system clock in KHz */
return(sysClk);
}
#else
Uint32 getSysClk(void)
{
Bool pllRDBypass;
Bool pllOutDiv;
Bool pllOutDiv2;
Uint32 sysClk;
Uint16 pllVP;
Uint16 pllVS;
Uint16 pllRD;
Uint16 pllVO;
Uint16 pllDivider;
Uint32 pllMultiplier;
pllVP = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR1, SYS_CGCR1_MH);
pllVS = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_ML);
pllRD = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDRATIO);
pllVO = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_ODRATIO);
pllRDBypass = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDBYPASS);
pllOutDiv = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_OUTDIVEN);
pllOutDiv2 = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_OUTDIV2BYPASS);
pllDivider = ((pllOutDiv2) | (pllOutDiv << 1) | (pllRDBypass << 2));
pllMultiplier = ((Uint32)CSL_PLL_CLOCKIN * ((pllVP << 2) + pllVS + 4));
switch(pllDivider)
{
case CSL_PLL_DIV_000:
case CSL_PLL_DIV_001:
sysClk = pllMultiplier / (pllRD + 4);
break;
case CSL_PLL_DIV_002:
sysClk = pllMultiplier / ((pllRD + 4) * (pllVO + 4) * 2);
break;
case CSL_PLL_DIV_003:
sysClk = pllMultiplier / ((pllRD + 4) * 2);
break;
case CSL_PLL_DIV_004:
case CSL_PLL_DIV_005:
sysClk = pllMultiplier;
break;
case CSL_PLL_DIV_006:
sysClk = pllMultiplier / ((pllVO + 4) * 2);
break;
case CSL_PLL_DIV_007:
sysClk = pllMultiplier / 2;
break;
}
/* Return the value of system clock in KHz */
return(sysClk/1000);
}
#endif