This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5535: How to Build TIesr API's using makefile without errors in ubntu 14.04

Part Number: TMS320C5535

hello

Recently I am working in speech Recognizer System. I am creating YES and NO words for recognizing which is given in README.txt file

In that I need to build all TIesr API's.I am working on  ubntu14.04

so to build all I am using the command  

"make LinuxDebugGnu  PROJECTS='TIesrDTso TestTIesrDT'

using this command I need to build the two indiduval projects.

But when I am using this command I am getting error as below

""

user@EESBLRP105:~/ti-1/TIesr_src/TIesr_model_build$ make LinuxDebugGnu  PROJECTS='TIesrDTso TestTIesrDT'
cd TIesrDT/TIesrDTso && make SUB=no CONF=LinuxDebugGnu  build
make[1]: Entering directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TIesrDTso'
"make" -f nbproject/Makefile-LinuxDebugGnu.mk QMAKE= SUBPROJECTS=NO .build-conf
make[2]: Entering directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TIesrDTso'
"make"  -f nbproject/Makefile-LinuxDebugGnu.mk ../../Dist/LinuxDebugGnu/lib/libTIesrDT.so.1
make[3]: Entering directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TIesrDTso'
make[3]: `../../Dist/LinuxDebugGnu/lib/libTIesrDT.so.1' is up to date.
make[3]: Leaving directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TIesrDTso'
make[2]: Leaving directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TIesrDTso'
if [ LinuxDebugGnu == LinuxDebugGnu -o \
    LinuxDebugGnu == LinuxDebugGnuCurrent -o \
    LinuxDebugGnu == LinuxReleaseGnu -o \
    LinuxDebugGnu == LinuxReleaseGnuCurrent -o \
    LinuxDebugGnu == ArmLinuxDebugGnueabi -o \
    LinuxDebugGnu == ArmLinuxReleaseGnueabi ]; \
    then mkdir -p ../../Dist/LinuxDebugGnu/lib; \
    cd ../../Dist/LinuxDebugGnu/lib; \
    rm -f libTIesrDT.so; \
    ln -s libTIesrDT.so.1 libTIesrDT.so; \
    fi
/bin/sh: 1: [: LinuxDebugGnu: unexpected operator
make[1]: Leaving directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TIesrDTso'
cd TIesrDT/TestTIesrDT && make SUB=no CONF=LinuxDebugGnu  build
make[1]: Entering directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TestTIesrDT'
make -f nbproject/Makefile-LinuxDebugGnu.mk SUBPROJECTS=NO .build-conf
make[2]: Entering directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TestTIesrDT'
make  -f nbproject/Makefile-LinuxDebugGnu.mk ../../Dist/LinuxDebugGnu/bin/testtiesrdt
make[3]: Entering directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TestTIesrDT'
mkdir -p ../../Dist/LinuxDebugGnu/bin
gcc -v    -o ../../Dist/LinuxDebugGnu/bin/testtiesrdt build/LinuxDebugGnu/GNU_current-Linux-x86/_ext/_DOTDOT/src/TestTIesrDT.o -L../../Dist/LinuxDebugGnu/lib -Wl,-rpath `pwd`/../../Dist/LinuxDebugGnu/lib -lTIesrDT
Using built-in specs.
COLLECT_GCC=gcc
COLLECT_LTO_WRAPPER=/usr/lib/gcc/x86_64-linux-gnu/4.8/lto-wrapper
Target: x86_64-linux-gnu
Configured with: ../src/configure -v --with-pkgversion='Ubuntu 4.8.4-2ubuntu1~14.04.3' --with-bugurl=file:///usr/share/doc/gcc-4.8/README.Bugs --enable-languages=c,c++,java,go,d,fortran,objc,obj-c++ --prefix=/usr --program-suffix=-4.8 --enable-shared --enable-linker-build-id --libexecdir=/usr/lib --without-included-gettext --enable-threads=posix --with-gxx-include-dir=/usr/include/c++/4.8 --libdir=/usr/lib --enable-nls --with-sysroot=/ --enable-clocale=gnu --enable-libstdcxx-debug --enable-libstdcxx-time=yes --enable-gnu-unique-object --disable-libmudflap --enable-plugin --with-system-zlib --disable-browser-plugin --enable-java-awt=gtk --enable-gtk-cairo --with-java-home=/usr/lib/jvm/java-1.5.0-gcj-4.8-amd64/jre --enable-java-home --with-jvm-root-dir=/usr/lib/jvm/java-1.5.0-gcj-4.8-amd64 --with-jvm-jar-dir=/usr/lib/jvm-exports/java-1.5.0-gcj-4.8-amd64 --with-arch-directory=amd64 --with-ecj-jar=/usr/share/java/eclipse-ecj.jar --enable-objc-gc --enable-multiarch --disable-werror --with-arch-32=i686 --with-abi=m64 --with-multilib-list=m32,m64,mx32 --with-tune=generic --enable-checking=release --build=x86_64-linux-gnu --host=x86_64-linux-gnu --target=x86_64-linux-gnu
Thread model: posix
gcc version 4.8.4 (Ubuntu 4.8.4-2ubuntu1~14.04.3)
COMPILER_PATH=/usr/lib/gcc/x86_64-linux-gnu/4.8/:/usr/lib/gcc/x86_64-linux-gnu/4.8/:/usr/lib/gcc/x86_64-linux-gnu/:/usr/lib/gcc/x86_64-linux-gnu/4.8/:/usr/lib/gcc/x86_64-linux-gnu/
LIBRARY_PATH=/usr/lib/gcc/x86_64-linux-gnu/4.8/:/usr/lib/gcc/x86_64-linux-gnu/4.8/../../../x86_64-linux-gnu/:/usr/lib/gcc/x86_64-linux-gnu/4.8/../../../../lib/:/lib/x86_64-linux-gnu/:/lib/../lib/:/usr/lib/x86_64-linux-gnu/:/usr/lib/../lib/:/usr/lib/gcc/x86_64-linux-gnu/4.8/../../../:/lib/:/usr/lib/
COLLECT_GCC_OPTIONS='-v' '-o' '../../Dist/LinuxDebugGnu/bin/testtiesrdt' '-L../../Dist/LinuxDebugGnu/lib' '-mtune=generic' '-march=x86-64'
 /usr/lib/gcc/x86_64-linux-gnu/4.8/collect2 --sysroot=/ --build-id --eh-frame-hdr -m elf_x86_64 --hash-style=gnu --as-needed -dynamic-linker /lib64/ld-linux-x86-64.so.2 -z relro -o ../../Dist/LinuxDebugGnu/bin/testtiesrdt /usr/lib/gcc/x86_64-linux-gnu/4.8/../../../x86_64-linux-gnu/crt1.o /usr/lib/gcc/x86_64-linux-gnu/4.8/../../../x86_64-linux-gnu/crti.o /usr/lib/gcc/x86_64-linux-gnu/4.8/crtbegin.o -L../../Dist/LinuxDebugGnu/lib -L/usr/lib/gcc/x86_64-linux-gnu/4.8 -L/usr/lib/gcc/x86_64-linux-gnu/4.8/../../../x86_64-linux-gnu -L/usr/lib/gcc/x86_64-linux-gnu/4.8/../../../../lib -L/lib/x86_64-linux-gnu -L/lib/../lib -L/usr/lib/x86_64-linux-gnu -L/usr/lib/../lib -L/usr/lib/gcc/x86_64-linux-gnu/4.8/../../.. build/LinuxDebugGnu/GNU_current-Linux-x86/_ext/_DOTDOT/src/TestTIesrDT.o -rpath /home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TestTIesrDT/../../Dist/LinuxDebugGnu/lib -lTIesrDT -lgcc --as-needed -lgcc_s --no-as-needed -lc -lgcc --as-needed -lgcc_s --no-as-needed /usr/lib/gcc/x86_64-linux-gnu/4.8/crtend.o /usr/lib/gcc/x86_64-linux-gnu/4.8/../../../x86_64-linux-gnu/crtn.o
/usr/bin/ld: cannot find -lTIesrDT
collect2: error: ld returned 1 exit status
make[3]: *** [../../Dist/LinuxDebugGnu/bin/testtiesrdt] Error 1
make[3]: Leaving directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TestTIesrDT'
make[2]: *** [.build-conf] Error 2
make[2]: Leaving directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TestTIesrDT'
make[1]: *** [.build-impl] Error 2
make[1]: Leaving directory `/home/user/ti-1/TIesr_src/TIesr_model_build/TIesrDT/TestTIesrDT'
make: *** [TestTIesrDT] Error 2

Please help me how I an reduce this error.