Other Parts Discussed in Thread: UCD9222, TMS320C6678
Hello again!
This time around I'm trying to reduce the power consumed by the c6678 DSP.
I've powered down as many power-domains as I can within software (according to SPRUGV4A) as well as power down all 8 C66x CorePac's (as shown in SPRUGW0).
With all cores in standyby (controlled using XDS560v2 and CCS5) I am drawing around 1.088A and with the above power-reductions running on all 8 cores, I can only reduce the EVM's power to 0.840A.
Is this a realistic power reduction? It seems very small considering I have supposedly (I may have done it incorrectly) made all 8 cores idle.
Any ideas/thoughts on how I can reduce the power of the device when it's not in use would be VERY helpful.
Thank you for you help!