This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 DDR3 termination

Guru 15520 points


Hi,

I have a question about C6678 DDR3 I/F.

Is there any termination inside the C6678 DDR3.
In C6678 IBIS model, it is written like follow:
* Rx mode, 45 ohm Half Termination (90ohm to Vtt)
* Rx mode 50 ohm Full Termination (50ohm to Vtt)

Is this means that there are either 45 or 50 ohm termination inside the C6678?

best regards,
g.f.

  • DDR3 includes on die termination (ODT) for the data bus interface.  The termination in the DDR memory is used for write accesses.  The termination in the C667x is used for reads.  Currently the documentation for the DDR3 controller states that the ODT for reads should always be full Thevenin termination. 

  • Hi, Bill

    Thank for the answer.

    I understand that there is termination in the C667x and used for read.
    So, is the termination value 50 ohm?

    By the way, I checked the DDR3 Controller User's Guide(SPRUGV8C),
    but can't find that the ODT for reads should always be full Thevenin termination.
    Where is it written?

    best regards,
    g.f.

  • Hi g.f.

    The impedance is determined by the value of the resistor you have connected to you PTV pin.  If you have the recommended 45.3 ohm resistor you will have a full Thevenin termination with 45ohms to VTT.

    The full Thevenin is selected by default by placing a 0x1 in the RD_LOCKAL_ODT field in the DDR_PHY_CNTL_1 registers.  You can find this in Table 4-25 of the DDR3 Memory Controller Users Guide.

    Regards, Bill

  • Hi Bill,

    Thank you so much.

    I now understand.

    best regards,

    g.f.