Other Parts Discussed in Thread: 66AK2H12
Hi,
After reading the Timer64P user guide (sprugv5a) the following question arose.
In the watchdog timer control register (WDTCR) there are two fields named WDKEY (table 5-7).
The first one (bit 31-16) is used to put the watchdog timer in an active state and to service the watchdog.
The second one (bit 13-12) is described as the "idle enable key bits". I have found this to be the first and only place
where this is mentioned. Is this used to stop the watchdog timer when it is in active state or how should I interpret "idle mode"?
Thanks,
Raymond