hello:
I am using NDK, I have 4 interrupt include network interrupt ,and I find that code in the .cfg:
Ecm.eventGroupHwiNum[0] = 7;
Ecm.eventGroupHwiNum[1] = 8;
Ecm.eventGroupHwiNum[2] = 9;
Ecm.eventGroupHwiNum[3] = 10;
This mean the event 4~31 wil be mapped to CPU interrupt 7,and event 31~62 mapped to CPU interrupt 8, and so on.
if my project have 4 event between 4~31, and It may happen that the 4 event come together, only one event can be serverd by the ISR,because 4 event use one ISR.
So other event may not be severed by the ISR,witch leads to event loss.
1.Now I don't want to use event Group, 4 event mapped to 4 ISRs! I remove the 4 lines event Group code, and the run my project, the net is not OK and interrupt does not work! Why??
2. if I want to achieve my idea, what need I do?
ThankS!