Hello all,
I am reading SPRUGS6C and on page 1-5 it says:
"The PCIe subsystem has only one interface link and this link can be used in ×1 or ×2 lane arrangements connecting to only one device. In other words, there exists no support for connecting to two devices in an ×1 arrangement because it has the support of a single interface link. This also means that it can not be used as a switch."
-Does that means I cant connect the C6678 EVM/PCIE0 to a PC (using AMC to PCIE adaptor) for PCIE boot while using PCIE1 to interface with an FPGA at the same time for example?...if so, what the 2 lanes are for?
-If DSP/PCIE is a RC, can an EP start transmission?. or an EP is a slave and RC must send a read memory to it?
Regards,
Murad