Hi Ti engineers,
Now I'm using the AIF2 module in LTE , CPRI mode. I want to connect the AIF2 with the FFTC by using the AT event for UL LTE symbol data. When AIF2 has fully received each AxCs one symbol data, I need to get a AT event to trigger the EDMA to handle all the AxC data.
But now I'm compusing about setup the AT Event register. How can I make sure that when the event is generated,
the AIF fully received all AxCs symbol data because of the fiber len? when the timer start to count , maybe the data is just on the fiber. I can only caculate the fiber delay and add it to the offset to make sure the event is correct? Is this the only way for my problem?
Thanks for your reply,
Regards,
ziyang