This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI DSP C6670 communication with Xilinx "vertex" FPGA SRIO (IP) GEN 2



Hi

Our usage is such that :-

There is a 6 - DSP "TI C6670" communication with Vertex FPGA via "6 - SRIO" Links respectively.  

Earlier we were using the TI C6670 DSP to communicate with vertex FPGA ---> SRIO Gen 1.

Now the FPGA guys have upgraded to SRIO GEN 2 "IP Interface" Vertex board.

 

Now problem we are facing is that :-

Using 2 DSP - FPGA SRIO links , At the first start up for both DSP and FPGA links are working fine but when ever DSP resets or reloads again , then the FPGA is not able to get SRIO LOCK " synchronize " though LINK and PORT state is OK. In this scenario using the NREAD transaction is fetching invalid data.

This behaviour happened only with one DSP, the other DSP works fine all the time.

Please guide me how to resolve the Issue.

 

Thanks and Regards,

Manav

 

 

 

  • Hi,

    Earlier we have 6 DSP communication with vertex FPGA using 6- SRIO " GEN 1" links  respectively.

    Now the FPGA guys have upgraded to SRIO GEN 2.

     

    Problem we are facing :-

    using the 2 DSP and FPGA communication via 2 SRIO links resp , at the first start up for DSP and FPGA both the links work fine but whenever the DSP is reset or reloads then the FPGA is not able to get the SRIO LOCK " Gets Synchronise" even though the LINK and PORT is status is OK.

    This happened only with one DSP but the other DSP works fine all the time.

    I tried with the other DSPs as well, only DSP 0 and DSP 5 works.

     

    Please guide me to resolve the Issue.

     

    Thanks, Manav

     

     

     

  • Hi Manav,

    Please provide the following information:

    1. Share your FPGA RapidIO Specification REV?

    2. DSPs SRIO configuration detail? (ports and baud rate)

    3. Have you running same code on all DSP's? 

    C6670 RapidIO Specification Revisions 2.1
            - Physical, transport, and logical layer separations (modular architecture)
            - IDLE1 sequence - short control symbol
            - 1.25, 2.5, 3.125, and 5.0 Gbaud lane rates with 1x and 4x link widths

    C6670 SRIO does not support IDLE2 sequences. Refer below link:

    http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/186561/671091.aspx#671091

    Thanks,

  • Hi Ganapathi,

     

    Thanks for the reply.

     

    1. Share your FPGA RapidIO Specification REV?

     ----> RapidIO Gen 2 Ver 1.7

    2. DSPs SRIO configuration detail? (ports and baud rate)

    ----> There are 6 DSP communicating with vertex FPGA via 6 SRIO links using

           # Port 0 in 1x mode at baud rate 3.125 Gbps.

            #DSP acts as a master and FPGA operates in slave mode.

            # Only Maintenance , Nread/Nwrite, Nwrite_R transactions Direct IO are supported.

    3. Have you running same code on all DSP's? 

    ---->Yes,  I am running the same code on all DSP's.

     

    Regards, Manav

     

  • Hi Manav,

    Please confirm your FPGA RapidIO Specification revision. i did not find the ver 1.7 on repiidIO side.

    Your DSP's silicon versions are same?

    Thanks,

  • Hi Ganapathi,

     

    1. Correction to the FPGA RapidIO Specification revision :-

    --> Its XILINX's LogiCore IP RapidIO Gen 2  designed to "RapidIO Gen 2.2" specification.

     2. DSP's silicon versions are same for "TI C6670 DSP's"

     

    Regards,

    Manav

     

    Regards,

    Manav

     

     

  • Hi,

    In above thread you told DSP0 and DSP5 are properly communicating with FPGA, that means the DSP driver code is fine.

    I think issue on your FPGA side.

    Thanks,

  • Hi Ganapathi,

    Thanks for the reply.

    Yes, Among the 6 DSPs (0,5) are properly communicating with FPGA.

    But the FPGA guys also replicated the same code to support the 6 SRIO Link interface.

    On testing,

    #1.  I have observed that remote SRIO Link (FPGA) for  DSP 0 &  DSP 5 comes UP quickly as compared to delayed link activation in DSP 1 to DSP 4, after reset and releasing the DSP image.

    Even the link comes UP for DSP 1 to 4 , it is not stable. executing a transaction shows hostport(-1).

     ---> your comment/suggestion

     #2. After getting the SRIO LINK state in Working, when we use the NREAD transaction it fetches the wrong data in the DSP whereas upon debugging in the FPGA side using the chip scope tool its shows the correct 0xaddr is requested and the correct data is responded.

     ---> your comment/suggestion

    #3 I have tried Executing the same NREAD transaction multiple times,

    Either it gives some junk values OR I can see the error msg "No LSU available" OR unexpected  LSU Transaction Completion Status - {0 - request timed out, 4 - unsupported transaction type / invalid programming encoding for one or more LSU register fields}

     ---> your comment/suggestion

    #4 How do I verify why Nread Transaction request timed out ?

    #5 What physical layer status registers should I monitor to troubleshoot this problem ?

     

    Regards,

    Manav