We are using a Keystone II in a project and need to assign MAC addresses to it. I see that there is unique MAC address burned into the Keystone. But there appears to be only one.
We will be using two Ethernet ports in a system and they will be used by the same ARM core. How do I obtain MAC addresses for each? Does the MAC address burned into the part actually represent a range? Would it be valid to use the same MAC address for both (or all 4) ports (they are going through a switch in the chassis)?
Thanks
Lance