Hi,
I'am work on communication between three DSP ( two as an EP and one as RC ) with PCIe.
the both EP send the interruption to the RC :
* EP1 send interrupt to the Core_0 of the RC ( the EP1 send MSI_0)
* EP2 send interrupt to the Core_1 of the RC ( the EP2 send MSI_1)
I launch the both Core ( 0 and 1 ) of the RC , then i launch the EP1 and an error appears in the console :
>> ti.sysbios.gates.GateMutex: line 92: assertion failure: A_badContext: bad calling context. See GateMutex API doc for details.
xdc.runtime.Error.raise: terminating execution
so, I want to know if it is possible to acheive this scenario : two EP send interrupt to two Core of RC ?
if yes, what is means the error displayed in the console ?
thank you,
Sincerely,
Zakaria.