This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hyperlink address translation



Hi.

I'm trying to use HyperLink to transfer data from a local EVM to a remote EVM, and then read that data on the remote EVM. I have been studying address translation, both from the HyperLink UG as well as from here (keystone-workshop.googlecode.com/.../Intro%20to%20Hyperlink.pdf).

As far as I understand, the value of rxsegsel  is determined by the maximum segment size, and is used to extract the segment look-up table index from the Rx address. The examples provided in the above linked document are inconsistent with my understanding of rxsegsel. In Remote (Rx) address Example 3, although rxsegsel = 9, only bits 27-25 are considered for the index, although the UG says that for rxsegsel = 9, bits 30-25 must be considered.

What is correct?

Thanks.