This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Change frequency on c6678

Hello,

 

I have been looking for how change the frequency on cores of c6678 and have some questions

1.- In my application, is interesting that when the cores have low workload, down the frequency (for example of 1.24GHz to 800MHz), can do, without reset the cores?

2.- For change the frequency is ALWAYS necessary access to GEL

3.- Can use SYSCLK for changing the frequency with go operation of sprugv2f?

4.-Is possible use DVFS in c6678? I don't see the information for this

And other different question

5.- In this post http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/100929 do reference of what smartreflex is only used by hardware, can modify the register VCNTLID?

 

Best Regards,

Luis

  • Hi,

    1.- In my application, is interesting that when the cores have low workload, down the frequency (for example of 1.24GHz to 800MHz), can do, without reset the cores?

    Yes.

    2.- For change the frequency is ALWAYS necessary access to GEL

    No. User can also initialize/modify the CPU frequency in our test application itself.

    Thanks,
  • Hi,

    Thanks for your answer.
    So, i can use a register? where can i look for this?
    Sorry, but i don't find

    Regards,
    Luis.
  • Hi,

    Take a look at platform.c file for core PLL initialization: \ti\pdk_C6678_1_1_2_6\packages\ti\platform\evmc6678l\platform_lib\src\

            /* PLLC module handle structure */
            if (p_flags->pll) {
    
                /* Set the Core PLL */
                /* Clear local data structures */
                memset(&pllc_hwSetup, 0, sizeof(PllcHwSetup));
    
                /* Setup PLLC hardware parameters */
                pllc_hwSetup.divEnable  = (CSL_BitMask32) (PLLC_DIVEN_PLLDIV2 |
                                                           PLLC_DIVEN_PLLDIV5 |
                                                           PLLC_DIVEN_PLLDIV8) ;
    
                /* Setup PLLC hardware parameters */        
                pllc_hwSetup.pllM       = 
                        (((p_config->pllm) ? p_config->pllm : PLATFORM_PLL1_PLLM_val) - 1);
                pllc_hwSetup.preDiv   = PLATFORM_PLL_PREDIV_val - 1;
                pllc_hwSetup.pllDiv2  = PLATFORM_PLLDIV2_val - 1;
                pllc_hwSetup.pllDiv5  = PLATFORM_PLLDIV5_val - 1;
                pllc_hwSetup.pllDiv8  = PLATFORM_PLLDIV8_val - 1;
                pllc_hwSetup.postDiv  = PLATFORM_PLL_POSTDIV_val -1;
    
                /* set Pll */
                status = CorePllcHwSetup (&pllc_hwSetup);
    
                if (status != CSL_SOK) {
                     platform_errno = PLATFORM_ERRNO_PLL_SETUP;
                    return ( (Platform_STATUS) Platform_EFAIL);
                }
    
                /* Read back */
                status = CorePllcGetHwSetup (&pllc_hwSetupRead);
    
                if (status != CSL_SOK) {
                    platform_errno = PLATFORM_ERRNO_PLL_SETUP;
                    return ( (Platform_STATUS) Platform_EFAIL);
                }

    Thanks,

  • Thanks for your answer.

    Other question: when change the frequency, how can I know when the frequency is stable?
    exist some register for that?

    Regards,
    Luis.
  • Luis,

    There is no register to read the PLL output stability. However some alternate ways are there to set the PLL clock stable and check if the PLL initialization done without any errors.

    1. If executing the PLL initialization sequence immediately after device power-up, you must allow time for the PLL to become stable. PLL stabilization time is 100 µs.

    2. Below are the reserved pins on the device which will indicate the status of the main PLL lock, DDR3 PLL lock and PA PLL lock. These pins can be checked to identify whether or not the device encountered the error condition.
    • RSV20 - COREPLLLOCK
    • RSV21 - DDR3PLLLOCK
    • RSV22 - PAPLLLOCK

    Regards,
    Senthil