Dear all,
We are working on C6657 and we try to configure the DDR3 following up the examples that provided by TI but in respect to the design requirements of our chip.
We have noticed that some times the DDR3 is unstable. In errata documet we went throught the DDR3 Automatic Leveling Issue advisor 3 and we want to apply the workaround 3 (Full Automatic leveling). Do you believe that this will solve the problem?
In section 3.3 I cannot understand what means "There must be no writes to any fixed ratio registers when full automatic leveling is used."
What are the differences in the configuration between the two ways of leveling?
The registers SDRAM_TIM_1, SDRAM_TIM_2, SDRAM_TIM_3 should be confugired in both of them?
Moreover , should be the registers 2 - 24 configured as well?
Best regards
George