This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 Unused DDR3 Configuration

As mentioned in another post, we are not using the DDR3 portion of the C6678. It was stated that the DVDD15 power input pins can be left floating.

We have found out that for internal clocking needs of the C6678, the DDRCLK input to the DSP must be active.

Does the AVDDA2 power input provide all the necessary power required for the DDR3 internal clocking needs?

Is the DVDD15 only used for I/O buffers but not the internal clocking and that is why those pins can be left floating?

Do these floating DVDD15 pins require any bypass capacitors?

One final question, should the PTV15 pin, normally a 45.3 ohm resistor to VSS, still be connected? If so, what is the approximate current through the resistor?

Thanks!

Bill