Hi,
I am using the C6670 and trying to load a large matrix in for the program to use at run-time.
I am using the 'load memory' function in CCS, and this works OK if I run the program, pause the program, then load, then play the program. If I try to load the memory before starting the program, which is what I need to do, the memory is wiped. Presumably this is due to some initialization?
Is there a way to load the memory before starting the program so that it persists?
And/or is there another way to load large vectors/matrices on the DSP? Simply writing them in .c files causes the compiler to grind to a halt.
Many thanks for your help!
David