Part Number: 66AK2H12
Other Parts Discussed in Thread: UCD74120, UCD9244
Team,
I got the feedback from an EVM's user that the Smartreflex might not be working accordingly on the K2H EVM.
I have seen already the below posts that explains why 2 Smartreflex interfaces (ARM side and DSP side for CVDD) are available on the EVM:
https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/411766
https://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/395850
And that the EVM's smartreflex topology should not be used on custom board (but rather the data manual and HW design guide should be followed instead).
Still could you please clarify the smartreflex implementation of the EVM?
- Looking at K2H_K2HEVM-HK_SCH_A104_Rev4_0.pdf:
The CVDD rail is showed as 1 single rail but I think that the ARM CVDD and DSP CVDD are separated as 2 UCD74120 are used.
-Are both VCNTLn and VCNTLnT interface functional on the EVM?
Or is only VCNTL (ie the one documented in the data manual) actively used?
-Measuring with a scope the VCNTLn does not show any activities. Why?
-Is smartreflex only implemented on the DSP portion of the CVDD on the EVM? And is the ARM CVDD rail kept at a constant value?
-Has the MCSDK and processor SDK SW some special workarround for the EVM that that would disable smartreflex for CVDD?
Thanks in advance.
Anthony