Part Number: 66AK2G02
Other Parts Discussed in Thread: OMAP-L137,
Section 4.5 of the datasheet, "Connections for Unused Pins", has some very cumbersome requirements for individual pullup or pulldown resistors on many pins when unused. The K2G EVM doesn't adhere to these requirements, so it appears that they are not really required.
The datasheet says
AC19 / L4 / AD1 / AD4 / AE6 / AE9 / M2 / N4 / M1 / M3 / N2 / P2 / N1 / P1 / T4 / T1 / D24 / C17 / L5 / AC25 / AD24 / L21 / L23
Each of these balls must be connected to GND through a separate external pull resistor if unused
Is this really true? For example, on the EVM SPI0_CLK, SPI0_SIMO, SPI_SOMI, and SPI0_SCSn0 (M2 / N4 / M1 / M3) are connected to an expansion header with no pulldowns on the EVM. This is an apparent violation of the datasheet requirement. And on the EVM RMII_REFCLK (D24) is connected to a test point with no pulldown, in apparent violation of the requirement.
I am surprised that TDI (L5) requires a pulldown, because it has not needed one on previous processors according to the XDS Target Connection Guide.
The datasheet also says
L3 / W1 / W3 / K4 / AE2 / AE4 / AD6 / AD9 / U5 / W5 / V6 / W4 / V5 / V4 / AD25 / AE24 / K21 / M23
These balls must be connected to the corresponding power supply through a separate external pull resistor if unused
Again, I am surprised that TCK (L3) and TMS (K4) require pullups, because they have not previously needed them according to the XDS Target Connection Guide.
Then the datasheet notes
The following balls are reserved: Y1 (RSV13) / AA1 (RSV14) / AB1 (RSV15) / AA2 (RSV16) / AB2 (RSV17) / AC1 (RSV18)
These balls must be connected to DVDD18 through a separate external pull resistor.
However in the K2GEVM schematic they are connected to test points or to non-stuffed resistors. Are they required to be connected to DVDD18 or not?
Then the datasheet notes
All other unused signal balls with a Pad Configuration Register can be left unconnected with their multiplexing mode set to GPIO input and internal pulldown resistor enabled.
Unused signal balls should only be connected to a pad on the PCB. No trace or via should be connected to the pad for an unused signal. If trace or a via is connected to an unused signal pad, an external pulling resistor is required. Failure to included an external resistor could result in a high current state which could damaged the IO cell.
Seriously? I haven't looked at these exhaustively, but one example I see in the EVM schematic is K2, which is connected to a test point and has no external pulling resistor.