Part Number: 66AK2G02
Hello,
SYSOSC_IN for the K2G is said to be able to be configured as a single-ended oscillator input for sourcing the main PLL clocks from an external oscillator. In this configuration, it is unclear what the allowable input voltage ranges are.
The supply for the pin is shown as DVDD18, and the I/O Voltage is shown as 1.8V; however, there is mention of a "3.3V Mode" in Table 5-14.
Is this pin 1.8V only, or can it be driven by a 3.3V source?
Jeff