Part Number: TMDSEVM6678
Other Parts Discussed in Thread: FFTLIB, MATHLIB
Tool/software: Code Composer Studio
Hello. I got problems trying to use openMP on EVM 6678.
My configuration:
--------------------------------------------------
TMDSEVM6678LE Rev.3B
OS: Windows 7 x64
CCS: 7.3.0.00019
PDK: 04.01.00.06
CG_XML 2.41.00
CTools Library 2.2.0.0
DSPLIB 3.4.0.0
EDMA3 LLD 2.12.05.29
FFTLIB 3.1.0.0
Framework Components 3.40.02.07
IMGLIB 3.1.1.0
IPC 3.46.02.04
LIBARCH 1.0.0.0
LINALG 1.2.0.0
MATHLIB 3.1.1.0
NDK 2.25.01.11
OpenMP 2.06.02.00
PDK C667X 2.0.7
Processor SDK RTOS C667X 04.01.00.06
SYS/BIOS 6.46.05.55
TI CGT 6x 8.1.3
UIA 2.00.06.52
XDAIS 7.24.00.04
XDCtools 3.32.01.22
--------------------------------------------------
1. I created an empty RTSC project (as I understand I must use rtsc project)
2. I enabled IPC, OpenMP and SYS/BIOS in Products tab in project properties
3. I enabled --omp and --multithread in Advanced Optimizations for C6000 Compiler
4. Copied 'hello.c' and 'omp_config.cfg' from 'c:\ti\openmp_dsp_c667x_2_06_02_00\packages\examples\hello_with_make\' to my project folder
So I got this error building the project:
**** Build of configuration Debug for project omp_rtsc ****
"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 4 all -O
gmake[1]: Entering directory 'C:/_Projects/workspace_v7/omp_rtsc/Debug'
'Building file: ../omp_config.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_32_01_22_core/xs" --xdcpath="C:/ti/ipc_3_46_02_04/packages;C:/ti/openmp_dsp_c667x_2_06_02_00/packages;C:/ti/bios_6_46_05_55/packages;C:/ti/pdk_c667x_2_0_7/packages;C:/ti/ccsv7/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p ti.platforms.evm6678 -r release -c "C:/ti/ti-cgt-c6000_8.1.3" "../omp_config.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring omp_config.xe66 from package/cfg/omp_config_pe66.cfg ...
subdir_rules.mk:19: recipe for target 'build-472138095-inproc' failed
js: "C:/_Projects/workspace_v7/omp_rtsc/omp_config.cfg", line 127: TypeError: Cannot read property "base" from undefined (C:/_Projects/workspace_v7/omp_rtsc/omp_config.cfg#127)
"./package/cfg/omp_config_pe66.cfg", line 188
gmake.exe: *** [package/cfg/omp_config_pe66.xdl] Error 1
js: "C:/ti/xdctools_3_32_01_22_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[1]: *** [build-472138095-inproc] Error 1
gmake: *** [build-472138095] Error 2
gmake[1]: Leaving directory 'C:/_Projects/workspace_v7/omp_rtsc/Debug'
subdir_rules.mk:16: recipe for target 'build-472138095' failed
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
What was done wrong?
I read threads with other OpenMP problems on forum, but there no solutions there. So the question is: how to create working openMP project? Is there any step-by-step manual to start?