Part Number: TMS320C6678
I'm gathering information about the maximum clock speed allowed for C6678 DSP.
Problems arise when consulting TI's official documentation:
I'm a little bit confused.
Which one is right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6678
I'm gathering information about the maximum clock speed allowed for C6678 DSP.
Problems arise when consulting TI's official documentation:
I'm a little bit confused.
Which one is right?
All TMS320C6678 support 1400 MHz clock speed. There is no limitations but you should pay attention on the power supply voltage - CVDD voltage range will be 0.9 V to 1.1 V for 1000-MHz and 1250-MHz devices and 0.95 V to 1.15 V for 1400-MHz device. For more details refer to data sheet:

BR
Tsvetolin Shulev