Part Number: TMS320C6678
Hi,
I have two C6678, and I use the SRIO example code in the STK. The example code and document is in this link.
My develop environment is CCS 5.4 and MCSDK 2.1.1.6.
I test the SRIO SWRITE transfer from one c6678 L2 to the other c6678 L2, the result is correct, completion code is 0.
But I got completion code '6' when I change the destination address to DDR (i.e. 0x80000000), I use memory browser to check the data in the DDR, it is correct, just completion code is wrong.
What is meaning about “Retry” DOORBELL response received, or Atomic Test-and-swap was not allowed (semaphore in use).
Thank you,
Snaku