Other Parts Discussed in Thread: CCSTUDIO
Dear Sir,
I want to update the FW code on 6437 EVM board.
I already study the document "spraag0d_Using the TMS320DM643x Bootloader"
And I also have the project codes from http://www-s.ti.com/sc/techlit/spraag0.zip
Actually, I have already erased the boot code in the NOR flash by using the sample code in "C:\CCStudio_v3.3\boards\evmdm6437_v2\tests\norflash".
I have problems in creating the .bin file.
I have already installed Perl 5.10.X.X.
But when I run the batch files under "\ais_utility\bin\" directory
It shows error message "genAIS is not an internal or external command, not an executable program or batch"
Can you show me how to create the .bin file with any App.out file?
Best Regards,
Eric Fang