This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 McBSP not able to configure the registers?

Other Parts Discussed in Thread: DM3730

I am using DM8148 EVM and the McBSP is not connected to anything, even I have configured McBSP Pin Mux properly.

I just want to have a dlb or alb enabled for a loopback test.

But I found I am not able to configure the McBSP registers, e.g., set RCR2 (0x47000018) to 0x80A1, but RCR2 is still a "0" value not changing. When I set SPCR2 (0x47000010) to 0x230, it shows 0x210. and so forth.

Is there any extra steps to enable McBSP, in addition to McBSP clock setup from PRCM?

And, I did not find this DM8148 McBSP support from Linux PSP of sdk_5_00_26.

 

Thanks in advance,

Philip