Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi:
We are using DM8148 McBSP port to connect to two seperate audio chips, one for RX and one for TX, they are working at different FS rate.
Since McBSP has seperate FS and CLK lines, so we can connect that way.
But when we are writing the drivers, we found we can only get RX and TX data going if we enable SRG. and there is only one SRG that we can either set to use RX FS or TX FS, but not both at the same time.
Please help us since we might need to change our hardware design if this is the case for McBSP on DM8148.
regards
--Zhigang