This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to enable McBSP in DM814X under linux kernel ?

Dear Experts,

We are using DM814X with EVM and Custom board.
There is McBSP interface on our board, we want to use McBSP as serial interface.
However, in Linux Kernel 2.6.37 (EZSDK5/DVRRDK3.0), there is no example to use McBSP in DM814X.

Where can I find driver/example code to enable McBSP in DM814X under linux kernel ?
Can McBSP be utilized like linux uart device?

thx ~

HB