This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

512MB memory map config for DM814x



Hi all,

I am currently bringing up a custom 512M dm8148 board.  The software components and PSP versions are the same as EZSDK 5.05.02.00.  I have followed the instructions on the following site:

http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map#Changing_Memory_Map_For_512MB_Board

The board is currently bootable, and M3 firmware loads properly.  However, the omx library hangs at line 991 in OmxRpc.c, on the call to RcmClient_create (It will do this when running gst-inspect on any "omx_" element).  I have read through a few postings, including this one that most closely matches my issue:

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/186056.aspx

This post as well as one other suggests that the xem3 files shipped with the EZSDK that support omx need to be updated and rebuilt to support the 512MB memory map.   A file named "ti814x_hdvpss_512M.xem3" is referenced in TI81XX_VPSS_Video_Driver_User_Guide.pdf but the other postings suggest that this file does not support omx. 

Is this correct?  Do the M3 files need to be rebuilt?  If so, what changes need to be made?  Since I only have the EZSDK I am not currently able to access or build the M3 source.  Perhaps there is a better way to do h264enc/aacenc/resize than using the omx/gst components?  Any help is appreciated.

Thanks,

Steve

  • Hi Steve,

    Steve Springman said:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/186056.aspx

    This post as well as one other suggests that the xem3 files shipped with the EZSDK that support omx need to be updated and rebuilt to support the 512MB memory map.

    Could you please be more precise where exactly in the above E2E thread is stated that the xem3 files shipped with the EZSDK (dm814x_hdvicp.xem3, dm814x_hdvpss.xem3) that support OMX need to be updated and rebuilt to support the 512MB memory map?

    http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map#Changing_Memory_Map_For_512MB_DM814x_Board

    I do not see requirement to change and rebuild the EZSDK xem3 firmwares when changing from the default 1GB memory map to 512MB map, these are the steps:

    Step 1: Update LISA Registers

    Step 2.1: Change Linux Memory size

    Step 2.2: Change Location of Video Frame Buffers

    Step 2.3: Update memory map for DSP

    Step 2.4: Update memory map for Linux side app

    Steve Springman said:
    A file named "ti814x_hdvpss_512M.xem3" is referenced in TI81XX_VPSS_Video_Driver_User_Guide.pdf but the other postings suggest that this file does not support omx. 

    ti814x_hdvpss_512M.xem3 file is when using PSP only (without using EZSDK).

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_VPSS_Video_Driver_User_Guide

    The usage of loading M3 firmware described in this userguide does not apply for M3 firmware coming from TI SDK package. Please check SDK document to get details information.

    For the TI814X/AM387X platform, two different M3 firmwares, ti814x_hdvpss_512M.xem3 and ti814x_hdvpss_1G.xem3 are provided to support 512M DDR3 EVM and 1GB DDR3 EVM. The 512M.xem3 can be used on 512MB PG1.0 EVM only while 1G.xem3 can only be used over 1GB DDR3 PG2.0 EVM.

    If ti814x_hdvpss_512M.xem3 is planned to be used over PG2.1 silicon, DMM_LISA_MAP_0/1/2/3 must be reconfigured with PG1_0_DMM_LISA_MAP_0/1/2/3 in the u-boot. The default DMM_LISA_MAP_0/1/2/3 setting does not support ti814x_hdvpss_512M.xem3.

    Note that we are updating DMM_LISA_MAP_0/1/2/3 registers for 512MB map in step 1 (Update LISA Registers) of the EZSDK memory map user guide!

    Refer also to the below E2E threads which are discussing DM814x 512MB + OMX:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/268450.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/265270.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/252768.aspx

    Best regards,
    Pavel

  • Hi Pavel,

    Thanks for the response.  To be specific, the quote I was referring to in:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/186056.aspx

    was from TI employee HardikShah posted May 08 2012 03:04 AM:

    HardikShah said:

    If you want to use only V4L2 caputure + V4L2 display + fbdev than ti814x_hdvpss_512M.xem3 is fine,  if you want to use encode/decode or any of OpenMax components you need to use dm814x_hdvpss_v4l2..xem3, but you need to recompile it for 512MB as by default its compiled for 1G.

    We have requirements for encode/decode.  There are 2 hdvpss firmwares shipped with the EZSDK:  dm814x_hdvpss_v4l2.xem3 and dm814x_hdvpss.xem3.  Do either of these need to be rebuilt to support the 512MB memory map?


    Thanks,

    Steve


  • Steve,

    Steve Springman said:
    There are 2 hdvpss firmwares shipped with the EZSDK:  dm814x_hdvpss_v4l2.xem3 and dm814x_hdvpss.xem3.  Do either of these need to be rebuilt to support the 512MB memory map?

    dm814x_hdvpss.xem3 firmware is when use OMX VFDC, VFPC and VFCC components.

    dm814x_hdvpss_V4l2.xem3 is when use V4L2.

    See ti-ezsdk_dm814x-evm_5_05_02_00/docs/DM814x_EZ_Software_Developers_Guide.pdf, section  6.12 How to change from OMX to V4L2 firmware for capture/display

    As you are planning to use OMX (not V4L2), you should use dm814x_hdvpss.xem3.

    Comparing the memory map for 1GB and 512MB, I can see difference only in HDVICP2 firmware:

    1GB : 7MB size, start at address 0x9DD00000

    512MB: 15MB size, start at address 0x9D500000

    But the steps for change to 512MB memory map does not include step for rebuilding HDVICP2 firmware:
    http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map#Changing_Memory_Map_For_512MB_DM814x_Board

    I can see that memory map for 1GB and 256MB have many difference in the firmware side. And we have statement that we should change/rebuilt the firmware when planning to use 256MB map:
    http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map#Changing_Memory_map_for_256MB_board

    BR
    Pavel



  • Hi Pavel,

    So perhaps there are no changes required to the M3 firmware files themselves...  Maybe then this issue is unrelated to the memory map.  I was able to turn on some more debug information.  Below is the output of a call to "gst-inspect omx_scaler."  The gst-inspect application hangs on the last line below.  Does anyone have any ideas?

    :~# gst-inspect omx_scaler
    Factory Details:
      Long name:    OpenMAX IL for OMX.TI.VPSSM3.VFPC.INDTXSCWB component
      Class:    Filter
      Description:    Scale video using VPSS Scaler module
      Author(s):    Brijesh Singh
      Rank:        primary (256)

    Plugin Details:
      Name:            omx
      Description:        OpenMAX IL
      Filename:        /usr/lib/gstreamer-0.10/libgstomx.so
      Version:        0.3
      License:        LGPL
      Source module:    gst-openmax
      Binary package:    gst-openmax source release
      Origin URL:        Unknown package origin

    GObject
     +----GstObject
           +----GstElement
                 +----GstOmxBaseFilter
                       +----GstOmxBaseVfpc
                             +----GstOmxScaler

    Implemented Interfaces:
      GstImplementsInterface
      GstOmx

    Pad Templates:
      SINK template: 'sink'
        Availability: Always
        Capabilities:
          video/x-raw-yuv
                     format: { NV12 }
                      width: [ 1, 2147483647 ]
                     height: [ 1, 2147483647 ]
                  framerate: [ 0/1, 2147483647/1 ]
          video/x-raw-yuv-strided
                     format: { NV12 }
                  rowstride: [ 0, 2147483647 ]
                      width: [ 1, 2147483647 ]
                     height: [ 1, 2147483647 ]
                  framerate: [ 0/1, 2147483647/1 ]

      SRC template: 'src'
        Availability: Always
        Capabilities:
          video/x-raw-yuv
                     format: { YUY2 }
                      width: [ 1, 2147483647 ]
                     height: [ 1, 2147483647 ]
                  framerate: [ 0/1, 2147483647/1 ]


    Element Flags:
      no flags set

    Element Implementation:
      Has change_state() function: 0x4063a0c0
      Has custom save_thyself() function: gst_element_save_thyself
      Has custom restore_thyself() function: gst_element_restore_thyself

    Element has no clocking capabilities.
    Element has no indexing capabilities.
    Element has no URI handling capabilities.

    Pads:
      SRC: 'src'
        Implementation:
          Has custom eventfunc(): gst_pad_event_default
          Has custom queryfunc(): gst_pad_query_default
          Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default
          Has getcapsfunc(): gst_pad_get_fixed_caps_func
          Has setcapsfunc(): src_setcaps
          Has acceptcapsfunc(): gst_pad_acceptcaps_default
        Pad Template: 'src'
      SINK: 'sink'
        Implementation:
          Has chainfunc(): 0x40638f4c
          Has custom eventfunc(): 0x4065cdac
          Has custom queryfunc(): gst_pad_query_default
          Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default
          Has setcapsfunc(): sink_setcaps
          Has acceptcapsfunc(): gst_pad_acceptcaps_default
        Pad Template: 'sink'

    Element Properties:
      name                : The name of the object
                            flags: readable, writable
                            String. Default: null Current: "omxscaler0"
      component-role      : Role of the OpenMAX IL component
                            flags: readable, writable
                            String. Default: null Current: null
      component-name      : Name of the OpenMAX IL component to use
                            flags: readable, writable
                            String. Default: null Current: "OMX.TI.VPSSM3.VFPC.INDTXSCWB"
      library-name        : Name of the OpenMAX IL implementation library to use
                            flags: readable, writable
                            String. Default: null Current: "libOMX_Core.so"
      use-timestamps      : Whether or not to use timestamps
                            flags: readable, writable
                            Boolean. Default: true Current: true
      input-buffers       : The number of OMX input buffers
                            flags: Entering OMX_Init: (void)

    Module<ti.omx> Entering<DomxInit> @line<142>
    Entered function:DomxCore_procInit
    SysLink_setup() complete
    Module<ti.omx> Entering<DomxCore_mapDomxCore2MultiProcId> @line<269>
    Module<ti.omx> Leaving<DomxCore_mapDomxCore2MultiProcId> @line<275> with error<0:ErrorNone>
    Module<ti.omx> Entering<OmxRpc_moduleRegisterMsgqHeap> @line<892>
    Module<ti.omx> Entering<DomxCore_mapDomxCore2MultiProcId> @line<269>
    Module<ti.omx> Leaving<DomxCore_mapDomxCore2MultiProcId> @line<275> with error<0:ErrorNone>
    Module<ti.omx> Entering<DmmDelegate_createIpcHeap> @line<181>
    Module<ti.omx> Leaving<DmmDelegate_createIpcHeap> @line<195> with error<0:ErrorNone>
    Module<ti.omx> @<OmxRpc_moduleRegisterMsgqHeap> @line<927> msg<Before MessageQ_registerHeap>
    Module<ti.omx> @<OmxRpc_moduleRegisterMsgqHeap> @line<932> msg<After MessageQ_registerHeap>
    Module<ti.omx> Leaving<OmxRpc_moduleRegisterMsgqHeap> @line<935> with error<0:ErrorNone>
    Module<ti.omx> Entering<DomxCore_mapDomxCore2MultiProcId> @line<269>
    Module<ti.omx> Leaving<DomxCore_mapDomxCore2MultiProcId> @line<275> with error<0:ErrorNone>
    Module<ti.omx> Entering<OmxRpc_moduleRegisterMsgqHeap> @line<892>
    Module<ti.omx> Entering<DomxCore_mapDomxCore2MultiProcId> @line<269>
    Module<ti.omx> Leaving<DomxCore_mapDomxCore2MultiProcId> @line<275> with error<0:ErrorNone>
    Module<ti.omx> Entering<DmmDelegate_createIpcHeap> @line<181>
    Module<ti.omx> Leaving<DmmDelegate_createIpcHeap> @line<195> with error<0:ErrorNone>
    Module<ti.omx> @<OmxRpc_moduleRegisterMsgqHeap> @line<927> msg<Before MessageQ_registerHeap>
    Module<ti.omx> @<OmxRpc_moduleRegisterMsgqHeap> @line<932> msg<After MessageQ_registerHeap>
    Module<ti.omx> Leaving<OmxRpc_moduleRegisterMsgqHeap> @line<935> with error<0:ErrorNone>
    Module<ti.omx> Entering<DomxCore_mapDomxCore2MultiProcId> @line<269>
    Module<ti.omx> Leaving<DomxCore_mapDomxCore2MultiProcId> @line<275> with error<0:ErrorNone>
    Module<ti.omx> Entering<OmxRpc_moduleRegisterMsgqHeap> @line<892>
    Module<ti.omx> Entering<DomxCore_mapDomxCore2MultiProcId> @line<269>
    Module<ti.omx> Leaving<DomxCore_mapDomxCore2MultiProcId> @line<275> with error<0:ErrorNone>
    Module<ti.omx> Entering<DmmDelegate_createIpcHeap> @line<181>
    Module<ti.omx> Leaving<DmmDelegate_createIpcHeap> @line<195> with error<0:ErrorNone>
    Module<ti.omx> @<OmxRpc_moduleRegisterMsgqHeap> @line<927> msg<Before MessageQ_registerHeap>
    Module<ti.omx> @<OmxRpc_moduleRegisterMsgqHeap> @line<932> msg<After MessageQ_registerHeap>
    Module<ti.omx> Leaving<OmxRpc_moduleRegisterMsgqHeap> @line<935> with error<0:ErrorNone>
    Module<ti.omx> @<DomxInit> @line<183> msg<Waiting for Ipc_attach to happen b/w slave cores>
    Module<ti.omx> @<DomxInit> @line<186> msg<Wait completed for Ipc_attach to happen b/w slave cores>
    Module<ti.omx> Entering<OmxRpc_moduleInitServer> @line<793>
    Module<ti.omx> Entering<omxrpc_rcm_server_create> @line<220>
    @ omxrpc_rcm_server_create: rcmServerName OmxRpcRcmServer_3, priority 14
    Module<ti.omx> @<omxrpc_rcm_server_create> @line<225> msg<Before RcmServer_Params_init>
    Module<ti.omx> @<omxrpc_rcm_server_create> @line<229> msg<After RcmServer_Params_init>
    Module<ti.omx> @<omxrpc_rcm_server_create> @line<232> msg<Before RcmServer_create>
    Module<ti.omx> @<omxrpc_rcm_server_create> @line<240> msg<After RcmServer_create>
    Module<ti.omx> Leaving<omxrpc_rcm_server_create> @line<241> with error<0:ErrorNone>
    Module<ti.omx> Entering<omxrpc_rcm_server_remote_fxn_register> @line<279>
    @ omxrpc_rcm_server_remote_fxn_register regFxnCategory 0
    Calling RcmServer_addSymbol(OmxRpcGetHandle)
    Calling RcmServer_addSymbol(OmxRpcFreeHandle)
    Calling RcmServer_addSymbol(OmxRpcCreateProxyLite)
    Calling RcmServer_addSymbol(OmxRpcGetHeapMemStats)
    Calling RcmServer_addSymbol(OmxRpcDeleteProxyLite)
    Module<ti.omx> Leaving<omxrpc_rcm_server_remote_fxn_register> @line<306> with error<0:ErrorNone>
    Module<ti.omx> Entering<omxrpc_rcm_server_start> @line<255>
    Module<ti.omx> @<omxrpc_rcm_server_start> @line<256> msg<Before RcmServer_start>
    Module<ti.omx> @<omxrpc_rcm_server_start> @line<258> msg<After RcmServer_start>
    Module<ti.omx> Leaving<omxrpc_rcm_server_start> @line<259> with error<0:ErrorNone>
    Module<ti.omx> Leaving<OmxRpc_moduleInitServer> @line<854> with error<0:ErrorNone>
    Module<ti.omx> Leaving<DomxInit> @line<208> with error<0:ErrorNone>
    Entered function:DomxCore_mapPhyAddr2UsrVirtual
    Entered function:DomxCore_mapPhyAddr2UsrVirtual
    Entered function:DomxCore_mapPhyAddr2UsrVirtual
    Leaving OMX_Init: retVal OMX_ERRORTYPE: 0

    Entered: OMX_GetHandle (0xc970c, OMX.TI.VPSSM3.VFPC.INDTXSCWB, 0xc9708, 0x4067bca8)
    Component OMX.TI.VPSSM3.VFPC.INDTXSCWB In table OMX.TI.VPSSM3.VFCC idx 0
    Component OMX.TI.VPSSM3.VFPC.INDTXSCWB In table OMX.TI.VPSSM3.VFDC idx 1
    Component OMX.TI.VPSSM3.VFPC.INDTXSCWB In table OMX.TI.VPSSM3.VFPC.DEIHDUALOUT idx 2
    Component OMX.TI.VPSSM3.VFPC.INDTXSCWB In table OMX.TI.VPSSM3.VFPC.DEIMDUALOUT idx 3
    Component OMX.TI.VPSSM3.VFPC.INDTXSCWB In table OMX.TI.VPSSM3.VFPC.NF idx 4
    Component OMX.TI.VPSSM3.VFPC.INDTXSCWB In table OMX.TI.VPSSM3.VFPC.INDTXSCWB idx 5
    Component OMX.TI.VPSSM3.VFPC.INDTXSCWB found idx: 5

    In OMX_GetHandle, component OMX.TI.VPSSM3.VFPC.INDTXSCWB, omxhandle 0xcdc30
    Module<ti.omx> Entering<OmxProxy_commonInit> @line<2491>
    Module<ti.omx> @<OmxProxy_commonInit> @line<2492> msg<OMX.TI.VPSSM3.VFPC.INDTXSCWB>
    Module<ti.omx> Entering<omxproxy_map_component_name2info> @line<747>
    Module<ti.omx> Leaving<omxproxy_map_component_name2info> @line<764> with error<0:ErrorNone>
    Module<ti.omx> Entering<omxproxy_get_component_custom_config_info> @line<784>
    Module<ti.omx> Leaving<omxproxy_get_component_custom_config_info> @line<801> with error<0:ErrorNone>
    Module<ti.omx> @<OmxProxy_commonInit> @line<2565> msg<Before OmxRpc_Params_init>
    Module<ti.omx> Entering<OmxRpc_Params_init> @line<93>
    Module<ti.omx> Leaving<OmxRpc_Params_init> @line<99> with error<0:ErrorNone>
    Module<ti.omx> @<OmxProxy_commonInit> @line<2569> msg<After OmxRpc_Params_init>
    Module<ti.omx> @<OmxProxy_commonInit> @line<2579> msg<Before OmxRpc_create>
    Module<ti.omx> Entering<OmxRpc_object_create> @line<109>
    Module<ti.omx> Entering<OmxRpc_Instance_init> @line<570>
    Module<ti.omx> Entering<omxrpc_module_init_client> @line<324>
    Entered function:omxrpc_module_init_client (2)
    Module<ti.omx> Entering<OmxRpc_rcmClientCreate> @line<976>
    Entered function:OmxRpc_rcmClientCreate (0x40781a78, OmxRpcRcmServer_2, 5)
    setting log mask for framework components
    Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<Before RcmClient_Params_init>
    Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<987> msg<After RcmClient_Params_init>
    Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<Before RcmClient_create>
    [t=0x00000004] [tid=0x40603000] ti.sdo.rcm.RcmClient: --> RcmClient_create: ()
    [t=0x0000005f] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x000000ad] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x000000f8] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x00000147] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x0000019c] [tid=0x40603000] ti.sdo.rcm.RcmClient: --> RcmClient_Instance_init: (obj=0xcde40)
    [t=0x000001f3] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x00000240] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x00000289] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x000002d9] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x00000320] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x0000036b] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x000003b3] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x00000403] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x00000449] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x00000494] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x000004db] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x0000052b] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x00000578] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x000005c3] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x0000060c] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x0000065c] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x000006a2] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x000006ed] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x00000734] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x00000784] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x000007cd] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x00001dd0] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x00001e2e] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x00001e80] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x00001ecb] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x00001f16] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x00001f5f] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x00001fae] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x00001ffb] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x0000204a] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x00002093] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x000020e3] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x0000212a] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x00002175] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x000021be] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x0000220d] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void
    [t=0x00002254] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> enter: (@4074fbfc)
    [t=0x0000229d] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- enter: @00000000
    [t=0x000022e5] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: --> leave: (@4074fbfc, @00000000)
    [t=0x00002334] [tid=0x40603000] ti.sdo.xdcruntime.linux.GateThreadSupport: <-- leave: void

  • Hi,


    In case this helps others, the solution to this issue is the firmware_loader command line option to disable i2c support.  Since we don't use the tvp encoder -i2c 0 needed to be passed to the firmware loader.  I had removed the kernel parameter i2c_mode=1 from vpss.ko parameter list but didn't realize this option needed to be added to the firmware loader as well.  Thus far it seems no modifications to the M3 firmware is required for the 512MB configuration, though some posts suggest that modifications are required. 


    Thanks,

    Steve