This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fixing calls to mutex_unlock in 5633.v4l2_patches

In the following post the 5633.v4l2_patches (download link here) were suggested for a stable v4l2 capture:

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/186865/672532.aspx#672532

In patch 0002-TI81xx-Video-Proxy-Same-containers-are-used-for-Queu.patch, a couple of calls to mutex_unlock where introduced that were never reached because they were after a return statement. Specifically in functions:

  • vidioc_querybuf() - from drivers/media/video/ti81xx/ti81xxvid_main.c
  • ti81xxvin_mmap() - from drivers/media/video/ti81xx/ti81xxvin_main.c

My suggested fix as follows:

Index: kernel/linux-2.6.37-psp04.04.00.01/drivers/media/video/ti81xx/ti81xxvid_main.c
===================================================================
--- kernel.orig/linux-2.6.37-psp04.04.00.01/drivers/media/video/ti81xx/ti81xxvid_main.c 2014-04-17 17:15:49.434424196 -0600
+++ kernel/linux-2.6.37-psp04.04.00.01/drivers/media/video/ti81xx/ti81xxvid_main.c 2014-04-17 17:24:18.746448071 -0600
@@ -1804,13 +1804,15 @@
{
struct ti81xxvideo_fh *fh = priv;
struct ti81xx_vidout_dev *vout = fh->voutdev;
+ int r = 0;

v4l2_dbg(1, debug, &vout->vid_dev->v4l2_dev,
"VIDOUT%d: query buffer\n",
vout->vid);
mutex_lock(&vout->lock);
- return videobuf_querybuf(&vout->vbq, b);
+ r = videobuf_querybuf(&vout->vbq, b);
mutex_unlock(&vout->lock);
+ return r;
}

static int vidioc_qbuf(struct file *file, void *priv,
Index: kernel/linux-2.6.37-psp04.04.00.01/drivers/media/video/ti81xx/ti81xxvin_main.c
===================================================================
--- kernel.orig/linux-2.6.37-psp04.04.00.01/drivers/media/video/ti81xx/ti81xxvin_main.c 2014-04-17 17:15:49.494424199 -0600
+++ kernel/linux-2.6.37-psp04.04.00.01/drivers/media/video/ti81xx/ti81xxvin_main.c 2014-04-17 17:25:42.802452009 -0600
@@ -2450,11 +2450,13 @@
struct ti81xxvin_fh *fh = filep->private_data;
struct ti81xxvin_instance_obj *inst = fh->instance;
struct ti81xxvin_buffer_obj *buf_obj = &(inst->buf_obj);
+ int r = 0;

ti81xxvin_dbg(2, debug, "ti81xxvin_mmap\n");
mutex_lock(&buf_obj->buf_lock);
- return videobuf_mmap_mapper(&buf_obj->buffer_queue, vma);
+ r = videobuf_mmap_mapper(&buf_obj->buffer_queue, vma);
mutex_unlock(&buf_obj->buf_lock);
+ return r;
}
/* TI81xx capture file operations */
static struct v4l2_file_operations hdvpss_fops = {

Regards,