This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uboot cpsw phy



Hi,

I have KSZ9031RNX phy using rgmii interface but the address is 0x3, does this work with existing generic phy driver ? I get failed to read bmcr, while doing tftp.

Thanks & Reagrds,

Mike

  • Mike,

    mike A said:
    I have KSZ9031RNX phy using rgmii interface but the address is 0x3

    I think you should update the code to apply this change.

    See the below links:

    http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#Miscellaneous_details

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/358952.aspx

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/247923.aspx

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/269151.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/353786.aspx

    mike A said:
    I get failed to read bmcr, while doing tftp.

    Please provide full boot up log.

    BR
    Pavel

  • Hi Pavel,

    Here is the complete boot log:

    DRAM:  2 GiB
    DCACHE:  Off
    MMC:   OMAP SD/MMC: 0
    Using default environment

    Loading 2nd stage U-Boot...
    Hit any key to stop autoboot:  0
    reading u-boot.bin

    178096 bytes read
    ## Starting application at 0x80800000 ...


    I2C:   ready
    DRAM:  2 GiB
    DCACHE:  On
    NAND:  HW ECC BCH8 Selected
    512 MiB
    MMC:   OMAP SD/MMC: 0
    Net:   Detected MACID:84:7e:40:f4:f1:12
    cpsw
    Hit any key to stop autoboot:  0
    DM814X#
    DM814X#mii info
    DM814X#mii dump 0
    Error reading from the PHY addr=00 reg=00

    DM814X#tftp
    phyid: ffffffff
    failed to read bmcr
    Using cpsw device
    TFTP from server 192.168.1.115; our IP address is 192.168.1.105
    Filename 'uImage'.
    Load address: 0x81000000
    Loading: *
    Abort
    DM814X#

    Thanks & Regards,

    Mike

  • Hi Pavel,

    Do I need to add driver support for that phy ? If not how do I add support for it to change phy address to 3 ?

    Thanks & Regards,

    Mike

  • Mike,

    mike A said:

    Here is the complete boot log:

    DRAM:  2 GiB
    DCACHE:  Off
    MMC:   OMAP SD/MMC: 0
    Using default environment

    Loading 2nd stage U-Boot...
    Hit any key to stop autoboot:  0
    reading u-boot.bin

    178096 bytes read
    ## Starting application at 0x80800000 ...


    I2C:   ready
    DRAM:  2 GiB
    DCACHE:  On
    NAND:  HW ECC BCH8 Selected
    512 MiB
    MMC:   OMAP SD/MMC: 0
    Net:   Detected MACID:84:7e:40:f4:f1:12
    cpsw
    Hit any key to stop autoboot:  0
    DM814X#
    DM814X#mii info
    DM814X#mii dump 0
    Error reading from the PHY addr=00 reg=00

    DM814X#tftp
    phyid: ffffffff
    failed to read bmcr
    Using cpsw device
    TFTP from server 192.168.1.115; our IP address is 192.168.1.105
    Filename 'uImage'.
    Load address: 0x81000000
    Loading: *
    Abort
    DM814X#

    Below is how I use the tftp command:

    Net:   <ethaddr> not set. Reading from E-fuse
    Detected MACID:90:d7:eb:d5:13:96
    cpsw
    Hit any key to stop autoboot:  0
    TI8148_EVM#setenv autoload no
    TI8148_EVM#dhcp
    link up on port 0, speed 100, full duplex
    BOOTP broadcast 1
    DHCP client bound to address 172.20.0.110
    TI8148_EVM#setenv serverip 172.20.1.195
    TI8148_EVM#setenv nfsserver 172.20.1.195
    TI8148_EVM#tftp 0x81000000 uImage
    link up on port 0, speed 100, full duplex
    Using cpsw device
    TFTP from server 172.20.1.195; our IP address is 172.20.0.110
    Filename 'uImage'.
    Load address: 0x81000000
    Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ####################
    done
    Bytes transferred = 2762004 (2a2514 hex)
    TI8148_EVM#

    Can you try this flow at your side? The serverip and nfsserver is the ip of your host PC.

    BR
    Pavel

  • Hi Pavel,

    The problem in first place is I am not able to read mii registers itself. If you look at my boot log you can see that error.

    Do I need to add support for the phy driver or the generic phy driver will work ? How can I change the phy address to 3 ?

    Thanks & Regards,

    Mike

  • Mike,

    mike A said:
    The problem in first place is I am not able to read mii registers itself. If you look at my boot log you can see that error.

    What do you mean by "mii registers"? Are these the DM814x EMAC registers? Or the external eth PHY registers? There is no mii command in u-boot.

    mike A said:
    Do I need to add support for the phy driver or the generic phy driver will work ?

    The u-boot ethernet driver is generic and should work fine.

    mike A said:
    How can I change the phy address to 3 ?

    See the below links:

    http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#Miscellaneous_details

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/358952.aspx

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/247923.aspx

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/269151.aspx

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/353786.aspx

    BR
    Pavel

  • Hi Pavel,

    Here is the o/p of mii command on 8148 evm:

    ti8148_evm#mii info
    PHY 0x00: OUI = 0x1374, Model = 0x07, Rev = 0x04,  10baseT, HDX
    PHY 0x01: OUI = 0x1374, Model = 0x07, Rev = 0x04, 1000baseT, FDX
    ti8148_evm#mii dump 1
    0.     (3100)                 -- PHY control register --
      (8000:0000) 0.15    =     0    reset
      (4000:0000) 0.14    =     0    loopback
      (2040:2000) 0. 6,13 =   b01    speed selection = 100 Mbps
      (1000:1000) 0.12    =     1    A/N enable
      (0800:0000) 0.11    =     0    power-down
      (0400:0000) 0.10    =     0    isolate
      (0200:0000) 0. 9    =     0    restart A/N
      (0100:0100) 0. 8    =     1    duplex = full
      (0080:0000) 0. 7    =     0    collision test enable
      (003f:0000) 0. 5- 0 =     0    (reserved)

    CONFIG_CMD_MII needs to enabled to get mii command.

    Thanks & Regards,

    Mike