Hi,
I am booting from NAND flash, after linux is booted I insert a sd card of FAT£2 the linux fails to detect it, If I do fdisk -l it doesnt show up any pointers on what could be missing ?
Thanks And Regards
Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mike,
I made a test in the past.
The test is made with:
1. DM8148 Mistral TI EVM
2. DM8148 silicon revision 2.1
3. EZSDK 5.05.02.00
4. PSP 04.04.00.01
5. Micro SDHC card, ADATA, 4GB (plugged into ADATA Micro SD adapter)
6. Boot u-boot (1st and 2nd stage) from UART, TFTP uImage through the EMAC port 0, NFS filesystem (targetfs)
When testing with the default EZSDK/PSP source code, the SD card can be identified for more then 10 times of pluging in and out rapidly. The MMC/SD hot insertion (plug) and hot removal feature seems to work fine. These are the messages, when make hot insertion:
root@dm814x-evm:~# mmc0: new high speed SDHC card at address 0002
mmcblk0: mmc0:0002 00000 3.70 GiB
mmcblk0: p1 p2
FAT: bogus number of reserved sectors
VFS: Can't find a valid FAT filesystem on dev mmcblk0.
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
Then the Enter is pressed, and the SDHC card can be accessed successfully. The SDHC card successful identification is reported through the below messages:
mmc0: new high speed SDHC card at address 0002
mmcblk0: mmc0:0002 00000 3.70 GiB
mmcblk0: p1 p2
These are the messages when make hot removal:
root@dm814x-evm:/# mmc0: card 0002 removed
EXT3-fs (mmcblk0p2): I/O error while writing superblock
Then the Enter is pressed, and the SDHC card is removed successfully.
Can you try to reproduce this issue on DM814x EVM? Is the issue valid only on your custom board?
Can you try with different MMC/SD card?
The below wiki pages states that MMC/SD hot plug/insert is supported:

Support:
MMC/SD card hot insertion and removal

The driver supports the following features:
5. MMC/SD card hot insertion and removal
See also if the below pointers will help:


BR
Pavel
Hi Pavel,
static struct omap2_hsmmc_info mmc[] = {
#ifdef CONFIG_WL12XX_PLATFORM_DATA
{
.mmc = 1,
.caps = MMC_CAP_4_BIT_DATA | MMC_CAP_POWER_OFF_CARD,
.gpio_cd = -EINVAL,
.gpio_wp = -EINVAL,
.ocr_mask = MMC_VDD_33_34,
.nonremovable = true,
},
#endif
{
.mmc = 2,
.caps = MMC_CAP_4_BIT_DATA,
.gpio_cd = -EINVAL, /* check setup_mmc2_pin_mux() */
.gpio_wp = -EINVAL,
.ocr_mask = MMC_VDD_33_34,
},
{} /* Terminator */
};
Do I need to add GPIO pins to detect the hot plug ? because I see cd is connected to GP1[6] and wp to GP1[3] ?
Thanks And Regards,
Mike
Mike,
mike A said:because I see cd is connected to GP1[6] and wp to GP1[3] ?
Where do you see this?
mike A said:Do I need to add GPIO pins to detect the hot plug ?
If not using the SD card connector CD pin, then yes, GPIO pin is needed. DM814x TI EVM is using MMC1/SD1 controller, connect SD1_SDCD/MMC1_SD_CD (pin AE5) to SD card connector CD pin 15, no GPIO is needed.
linux-kernel/arch/arm/mach-omap2/board-ti8148evm.c
static struct omap2_hsmmc_info mmc[] = {
{
.mmc = 2,
.caps = MMC_CAP_4_BIT_DATA,
.gpio_cd = -EINVAL, /* check setup_mmc2_pin_mux() */
.gpio_wp = -EINVAL,
.ocr_mask = MMC_VDD_33_34,
},
{} /* Terminator */
};
I see that GPIO pin for CD is used in J5Eco/TI811x EVM and DM814x IPNC board:
linux-kernel/arch/arm/mach-omap2/board-ti811xevm.c
static struct omap2_hsmmc_info mmc[] = {
{
.mmc = 1,
.caps = MMC_CAP_4_BIT_DATA,
.gpio_cd = GPIO_TO_PIN(1, 6), /* Dedicated pins for CD and WP */
.gpio_wp = GPIO_TO_PIN(1, 3),
.ocr_mask = MMC_VDD_33_34,
},
{} /* Terminator */
};
linux-kernel/arch/arm/mach-omap2/board-ti8148ipnc.c
static struct omap2_hsmmc_info mmc[] = {
{
#ifdef CONFIG_WL12XX_PLATFORM_DATA
/* WLAN_EN is GP2[22] */
#define GPIO_WLAN_EN ((2 * 32) + 22)
/* WLAN_IRQ is GP2[24] */
#define GPIO_WLAN_IRQ ((2 * 32) + 24)
.mmc = 1,
.caps = MMC_CAP_4_BIT_DATA | MMC_CAP_POWER_OFF_CARD,
.gpio_cd = -EINVAL,
.gpio_wp = -EINVAL,
.ocr_mask = MMC_VDD_165_195,
.nonremovable = true,
},
{
.mmc = 2,
#else
.mmc = 1,
#endif
.caps = MMC_CAP_4_BIT_DATA,
.gpio_cd = 79,/* Dedicated pins for CD and WP */
.gpio_wp = 80,
.ocr_mask = MMC_VDD_33_34,
},
{} /* Terminator */
};
BR
Pavel