This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need to cross-compile QT5.5 for DM8127



Hi All,

I have a requirement of porting QT5.5 libraries on DM8127. We are using IPNC_RDK_3.8.0 and arm-arago toolchain.

I tried to cross-compile QT5.5, with the toolchain specifications, but could not get any success. QT 5.5 by default enables support for OpenGL, which is not readily available in library form with IPNC_RDK. We also want to use webkit module, with our QT application, so required to configure QT5.5 with webkit support enabled.

I wonder if anyone has already cross-compiled QT5.5 with arm-arago toolchain and sucessfully ported it to DM8127 platform and can guide me with some steps.

Any help would be highly appreciated.

Thanks,

Krinali Shah