This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x: Problems with capturing an image from CPI into RAM

Hello all,

I have some trouble to transfer images from the camera parallel interface into RAM using the ISS of a DM8147 on our custom board.

I followed the instructions in SPRUH30B "TMS320DM814x Imaging Subsystem (ISS) User's Guide", chapter 3.4.1.1.2 "ISS ISP ISIF Register Setup".

Our camera is connected to the CPI camera parallel interface providing a pixel clock of 25 MHz.


Obviously some data are received by the ISS. When checking the HS/VS IRQs is see a proper number of HS/VS IRQs matching the number of lines or images respectively.


But that's all I could see so far. The image is not put into memory to the address configured by ISIF_CADU/ISIF_CADL registers. And the VDINT IRQs don't occur  as configured by ISIF_VDINT0/ISIF_VDINT1 register.

I would greatly appreciate any help what to check next - settings or data that should change when an image is received. Thanks in advance.

Best regards,

Lars