Part Number: TMS320DM8148
Other Parts Discussed in Thread: TVP5150
Tool/software: Linux
I am seeing color bleeding from the bottom of imagery to top when capturing YUV data in NV12 format. This problem does not exist when capturing in YUYV mode
It appears that the Luma component from the bottom of the image is being displayed as Croma near the top of the image. I often see the purple and green colors when Luma/Chroma are swapped.
The issue is very similar to this posting:
https://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/382147/1346533
-> I have discovered that if the camera outputs at least 30 lines of vertical blanking, that the problem goes away. This is the case for both embedded sync systems (like HD-SDI) as well as discrete VSync/Hsync line capture.
-> Can you point me to the relevant code (I think on M3 processor) where the addressing is being setup for NV12 capture. I think there is a bug in there.
Thanks, Steve