connected a 1366x768 LCD panel to the DM8168, running 5.02 sdk. referencing:
I'm trying to get the correct timing/VPSS to use the LCD. I believe I'm correctly connected electrically as I'm getting a partial/ghosted image on the panel.
So far, I've routed /sys/devices/platform/vpss/graphics0/nodes to 1:dvo2, set display1/timings to various ~75mhz/front/back porch tries of 1366x768. It seems that the VPSS unit is fixed to versions of 1280x720, as the bottom, and right sides of the LCD are blacked out. Is this a hard-coded limitation of the current VPSS driver?
-Dal