This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omx_videomixer to mix png image file and video file



Hi All,

I'm using following pipeline to mix png image with video file.

gst-launch omx_videomixer name=mix \
        ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60 ! gstperf \
        ! omx_videosink sync=false  \
        filesrc location=Sample.mp4 ! 'video/x-h264' \
        ! h264parse access-unit=true ! omx_h264dec ! mix. \
    filesrc location=Sample.png \
    ! pngdec ! queue ! ffmpegcolorspace \
    ! imagefreeze !  mix.

The output of gst-launch command.

In base init!!
In class init!!
In instance init!!
queue_0 : 0x147e98
queue_1 : 0x147eb0
queue_2 : 0x147ec8
queue_3 : 0x147f00
In instance init/...done!!
Setting pipeline to PAUSED ...
Video mixer activate push!!
Pipeline is PREROLLING ...
In sink set caps:video/x-raw-yuv, format=(fourcc)NV12, width=(int)866, height=(int)90, framerate=(fraction)25/1
Starting input thread!!
omx_setup!!
omx_setup...done!!

As you can notice, the pipeline waits in 'PREROLLING' state and does not transit in PLAYING state. I tested omx_videomixer with single video file and got same result. Even for single video file, PIPELINE did not transit to PLAYING state.

1. Is omx_videomixer immature element in EZSDK-5.3.1.15 ?

2. Is it necessary to upgrade EZSDK to 5.5.2.0 version to use omx_videomixer?

Thanks,

Rajnikant

E2E http://www.ti.com/e2e-community

  • Hello,

    Rajnikant Jachak said:
    Is omx_videomixer immature element in EZSDK-5.3.1.15 ?


    EZSDK-5.3.1.15 omx_videomixer gstreamer element implementation is hardcoded for 4 inputs. So you need to give 4 inputs for it to work. To get the videomixer working, you would have to patch it too.

    please try with the latest EZSDK version 5_05_02_00.

    Best Regards,

    Margarita

  • Hello Margarita,

    I tried latest ezsdk (5_05_02_00) on dm814x EVM board. But now board is not booting up.

    Following are the boot logs which I captured from my minicom terminal:

    Mon Dec 31 10:37:00 UTC 2012
    INIT: Entering runlevel: 5
    Loading HDVICP2 Firmware
    DM814X prcm_config_app version: 2.0.0.1
    Doing PRCM settings...
            PRCM for IVHD0 is in Progress, Please wait.....  
                            BW Phy Addr : 0x48180600 Data : 0x00000001
                            AW Phy Addr : 0x48180600 Data : 0x00000002
                            Phy Addr : 0x48180c04 Data : 0x00000037
                    Data : 0x00000007
                            AW Phy Addr : 0x48180c10 Data : 0x00000003
                            Phy Addr : 0x48180c14 Data : 0x00000004
                            BW Phy Addr : 0x58088000 Data : 0xd17dcf5c
                            AW Phy Addr : 0x58088000 Data : 0xeafffffe
                            BW Phy Addr : 0x58098000 Data : 0x8fd19924
                            AW Phy Addr : 0x58098000 Data : 0xeafffffe
                            BW Phy Addr : 0x48180c10 Data : 0x00000003
                            AW Phy Addr : 0x48180c10 Data : 0x00000000
                            Phy Addr : 0x48180c14 Data : 0x00000007
            PRCM for IVHD0 is Done Successfully  
    PRCM Initialization completed
    SysLink version : 2.20.02.20
    SysLink module created on Date:Dec 26 2012 Time:18:39:49
    FIRMWARE: I2cInit will be done by M3
    FIRMWARE: Memory map bin file not passed
    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
    ===Mandatory arguments===
    <Processor Id>         0: DSP, 1: Video-M3, 2: Vpss-M3
    <Location of Firmware> firmware binary file
    <start|stop>           to start/stop the firmware
    ===Optional arguments===
    -mmap                  input memory map bin file name
    -i2c                   0: i2c init not done by M3, 1(default): i2c init done by M3
    FIRMWARE: isI2cInitRequiredOnM3: 1
    FIRMWARE: Default memory configuration is used
    Firmware Loader debugging not configured
    Default FL_DEBUG: warning
    Allowed FL_DEBUG levels: error, warning, info, debug, log
    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.2.1
    vmap allocation for size 197136384 failed: use vmalloc=<size> to increase size.
    Unable to handle kernel paging request at virtual address 40000010
    pgd = ef1b0000
    [40000010] *pgd=af09b031, *pte=00000000, *ppte=00000000
    Internal error: Oops: 817 [#1]
    last sysfs file: /sys/kernel/uevent_seqnum
    Modules linked in: syslink ipv6
    CPU: 0    Not tainted  (2.6.37 #1)
    PC is at HeapMemMP_postInit+0x178/0x228 [syslink]
    LR is at GateMP_getSharedAddr+0x4c/0x60 [syslink]
    pc : [<bf099d84>]    lr : [<bf095f38>]    psr: 80000013
    sp : ef18bd78  ip : 00000000  fp : ef18bdb4
    r10: 00000001  r9 : ef18be14  r8 : ef18be00
    r7 : f0807000  r6 : f080a000  r5 : 40000000  r4 : 0bbfff80
    r3 : 00000580  r2 : 00000580  r1 : 00060000  r0 : 00000580
    Flags: Nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
    Control: 10c5387d  Table: af1b0019  DAC: 00000015
    Process firmware_loader (pid: 2054, stack limit = 0xef18a2e8)
    Stack: (0xef18bd78 to 0xef18c000)
    bd60:                                                       00000002 00000004
    bd80: ef18bdb4 ef18bd90 ef18bdb4 ef18bd98 bf083264 bf074358 40000000 f080a000
    bda0: f0807000 00000000 ef18bdf4 ef18bdb8 bf09b63c bf099c18 ef18be00 00000001
    bdc0: ef18bdf4 00000000 bf0809ac ef18be00 ef18be44 f0b51048 00000000 00000002
    bde0: 00000048 00000000 ef18be2c ef18bdf8 bf09bfa0 bf09b250 f0b51048 00000002
    be00: 00000000 00000000 40000000 0bbfff80 00000000 f0807000 0bc00000 ef18be44
    be20: ef18be84 ef18be30 bf085764 bf09be74 ef18beb8 ef1b1338 ef18bea4 f0b51000
    be40: 00000001 00000000 00000000 40000000 0bbfff80 00000000 bf075630 c024f2a0
    be60: eee19280 be80aa64 00000009 be80aa64 ef18a000 00000000 ef18bef4 ef18be88
    be80: bf0c8218 bf085488 c024f2a0 be80aa64 ef18beac ef18bea0 c00bc1dc c00b3214
    bea0: ef18becc ffffffff 41266000 b3d00000 b3d00000 be80aa9c 40000000 0bc00000
    bec0: 00010003 00000000 00000080 00000001 00000000 00000000 00000000 eee19280
    bee0: 00000009 00000009 ef18bf04 ef18bef8 c00d76ec bf0c7dcc ef18bf74 ef18bf08
    bf00: c00d7dfc c00d76d0 000000fb 000000fb 41266000 ef348c80 ef123180 0bc00000
    bf20: 0000bc00 000b3d00 ef18bf74 ef18bf38 c00be258 c00bdbe0 000000fb 000b3d00
    bf40: ef18a000 ef348c80 00000001 00000000 be80aa64 c024f2a0 00000009 eee19280
    bf60: ef18a000 00000000 ef18bfa4 ef18bf78 c00d7e94 c00d7908 00000001 00000001
    bf80: 00000003 00046ee8 00000000 00008e20 00000036 c0047fa8 00000000 ef18bfa8
    bfa0: c0047e00 c00d7e48 00046ee8 00000000 00000009 c024f2a0 be80aa64 00000009

    eth0: no IPv6 routers present

    The boot process did not proceed after 'eth0: no IPv6 routers present' message.

    Could you please suggest how to resolve this?

    Thanks,

    Rajnikant

  • Hello Rajnikant,

    Rajnikant Jachak said:
    vmap allocation for size 197136384 failed: use vmalloc=<size> to increase size.
    Unable to handle kernel paging request at virtual address 40000010
    pgd = ef1b0000
    [40000010] *pgd=af09b031, *pte=00000000, *ppte=00000000
    Internal error: Oops: 817 [#1]


    Could you post yours bootargs.

    Best Regards,

    Margarita

  • Following are bootargs

    bootargs=console=ttyO0,115200n8 rootwait rw mem=364M@0x80000000 mem=320M@0x9FC00000 root=/dev/nfs nfsroot=10.1.1.243: ip=dhcp

    Thanks

  • Hello,

    Refer to this topic:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/236732/837484.aspx#837484

    To solve the problem you would need at least 400M vmalloc space to be set  in your bootargs.

    Best Regards,

    Margarita

  • Hi Margarita,

    I have upgraded EZSDK to 'ezsdk_5_05_02_00' version and tried using omx_videomixer for following pipeline, but it gave error.

    gst-launch  -v \
        omx_videomixer name=mix \
        ! omx_ctrl \
        ! omx_videosink sync=true \
        filesrc location=M2959_1_ENG_3_5.png \
        ! pngdec ! ffmpegcolorspace  \
        ! imagefreeze \
        ! mix. \
        filesrc location=Dabang_4_1080p24_unscrambled_H264.mp4 ! qtdemux \
        ! queue ! h264parse ! omx_h264dec ! gstperf print-arm-load=1 ! omx_scaler \
        ! ffmpegcolorspace \
        ! mix.

    --------------------------------- ERROR ------------------------------------

    (gst-launch-0.10:1555): GLib-GObject-WARNING **: invalid cast from `GstBuffer' to `GstOmxBufferTransport'
    Caught SIGSEGV accessing address (nil)
    perf0: frames: 15       current: 6.06    average: 6.06  arm-load: 11
    Spinning.  Please run 'gdb gst-launch 1555' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.

    So do I still need to patch omx? If yes where should I find patch?

    Thanks,

  • Hello,

    I will check it.

    Rajnikant Jachak said:
    gst-launch  -v \
        omx_videomixer name=mix \
        ! omx_ctrl \
        ! omx_videosink sync=true \
        filesrc location=M2959_1_ENG_3_5.png \
        ! pngdec ! ffmpegcolorspace  \
        ! imagefreeze \
        ! mix. \
        filesrc location=Dabang_4_1080p24_unscrambled_H264.mp4 ! qtdemux \
        ! queue ! h264parse ! omx_h264dec ! gstperf print-arm-load=1 ! omx_scaler \
        ! ffmpegcolorspace \
        ! mix.

    Could you try :

    gst-launch omx_videomixer name=mix  ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60 ! gstperf ! omx_videosink  filesrc location=sample2.mp4 ! qtdemux name=demux demux.audio_00 ! queue ! faad ! alsasink demux.video_00 ! queue ! h264parse ! omx_h264dec  ! mix.           ....    

    Best Regards,

    Margarita

  • Hello,

    You could check and this pipeline with videomixer:

    gst-launch --gst-debug=3 --verbose omx_videomixer framerate=15 port-index=0 name=mix ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60 ! gstperf ! omx_videosink sync=false filesrc location=/usr/share/ti/data/videos/dm816x_1080p_demo.264 ! 'video/x-h264' ! h264parse access-unit=true ! omx_h264dec ! mix. filesrc location=/usr/share/ti/data/videos/dm816x_1080p_demo.264 ! 'video/x-h264' ! h264parse access-unit=true ! omx_h264dec ! mix. filesrc location=/usr/share/ti/data/videos/dm816x_1080p_demo.264 ! 'video/x-h264' ! h264parse access-unit=true !  omx_h264dec ! gstperf ! mix.

    Best Regards,

    Margarita

  • Thanks Margarita.

    The above pipeline gave me following error:

    ------------------------------------- ERROR ----------------------------------

    /GstPipeline:pipeline0/GstOmxH264Dec:omxh264dec0.GstPad:src: caps = video/x-raw-yuv-strided, width=(int)1920, height=(int)1080, format=(fourcc)NV12, rowstride=(int)2048, interlaced=(boolean)false, framerate=(fraction)0/1
    OMX_EventError: 0x80001000
    unrecoverable error: There were insufficient resources to perform the requested operation (0x80001000)
    0:00:01.763601601  1513 0x503009e0 WARN                     omx gstomx_base_filter.c:708:pad_chain:<omxh264dec2> error: Error from OpenMAX component
    ERROR: from element /GstPipeline:pipeline0/GstOmxH264Dec:omxh264dec2: GStreamer encountered a general stream error.
    Additional debug info:
    gstomx_base_filter.c(708): pad_chain (): /GstPipeline:pipeline0/GstOmxH264Dec:omxh264dec2:
    Error from OpenMAX component
    ERROR: pipeline doesn't want to preroll.
    Setting pipeline to NULL ...
    0:00:01.765686351  1513 0x503009e0 WARN                 basesrc gstbasesrc.c:2574:gst_base_src_loop:<filesrc2> error: Internal data flow error.
    0:00:01.765787451  1513 0x503009e0 WARN                 basesrc gstbasesrc.c:2574:gst_base_src_loop:<filesrc2> error: streaming task paused, reason error (-5)

    I checked with 2 video input for mixer and it ran wel with 299M memory and avg 45% CPU.

    I want to display subtitles on my video and my subtitles are image files (png format). So I am thinking of using omx_videomixer to mix these two files and get desired effect.

    Can  I achieve this using omx_videomixer? we have achieved same by using following pipeline on linux desktop:

    gst-launch  -v \
        videomixer name=mix sink_1::xpos=520 sink_1::ypos=960 sink_1::alpha=0.3 sink_1::zorder=3 sink_2::xpos=400 sink_2::ypos=100 sink_2::zorder=2 background=3 \
        ! xvimagesink sync=true \
        filesrc location=M2959_1_ENG_3_5.png \
        ! pngdec ! queue ! ffmpegcolorspace \
        ! imagefreeze !  mix. \
        filesrc location=Dabang_4_1080p24_unscrambled_H264.mp4 \
        ! qtdemux ! queue \
        ! legacyh264parse ! queue ! ffdec_h264 \
        ! ffmpegcolorspace \
        ! mix.

    Thanks

  • Hello,

    This pipeline works for me.

    Margarita Gashova said:
    gst-launch --gst-debug=3 --verbose omx_videomixer framerate=15 port-index=0 name=mix ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60 ! gstperf ! omx_videosink sync=false filesrc location=/usr/share/ti/data/videos/dm816x_1080p_demo.264 ! 'video/x-h264' ! h264parse access-unit=true ! omx_h264dec ! mix. filesrc location=/usr/share/ti/data/videos/dm816x_1080p_demo.264 ! 'video/x-h264' ! h264parse access-unit=true ! omx_h264dec ! mix. filesrc location=/usr/share/ti/data/videos/dm816x_1080p_demo.264 ! 'video/x-h264' ! h264parse access-unit=true !  omx_h264dec ! gstperf ! mix.

    perf0: frames: 84     current: 31.99     average: 27.62    arm-load: 46
    perf1: frames: 101     current: 32.00     average: 25.03    arm-load: 47
    perf0: frames: 117     current: 32.01     average: 28.73    arm-load: 43
    perf1: frames: 133     current: 31.87     average: 26.39    arm-load: 42
    perf0: frames: 149     current: 31.80     average: 29.34    arm-load: 47

    Rajnikant Jachak said:
    GstPipeline:pipeline0/GstOmxH264Dec:omxh264dec0.GstPad:src: caps = video/x-raw-yuv-strided, width=(int)1920, height=(int)1080, format=(fourcc)NV12, rowstride=(int)2048, interlaced=(boolean)false, framerate=(fraction)0/1
    OMX_EventError: 0x80001000
    unrecoverable error: There were insufficient resources to perform the requested operation (0x80001000)
    0:00:01.763601601  1513 0x503009e0 WARN                     omx gstomx_base_filter.c:708:pad_chain:<omxh264dec2> error: Error from OpenMAX component
    ERROR: from element /GstPipeline:pipeline0/GstOmxH264Dec:omxh264dec2: GStreamer encountered a general stream error.
    Additional debug info:
    gstomx_base_filter.c(708): pad_chain (): /GstPipeline:pipeline0/GstOmxH264Dec:omxh264dec2:
    Error from OpenMAX component
    ERROR: pipeline doesn't want to preroll.
    Setting pipeline to NULL ...
    0:00:01.765686351  1513 0x503009e0 WARN                 basesrc gstbasesrc.c:2574:gst_base_src_loop:<filesrc2> error: Internal data flow error.
    0:00:01.765787451  1513 0x503009e0 WARN                 basesrc gstbasesrc.c:2574:gst_base_src_loop:<filesrc2> error: streaming task paused, reason error (-5)

    Could you post your bootargs?

    Rajnikant Jachak said:

    I want to display subtitles on my video and my subtitles are image files (png format). So I am thinking of using omx_videomixer to mix these two files and get desired effect.

    Can  I achieve this using omx_videomixer?

    I will check it and I will let you know the result.

    Best Regards,

    Margarita

  • These are my bootargs:

    console=ttyO0,115200n8 rootwait rw mem=256M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti814xfb.v
    ram=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=10.1.1.243:/opt/targetfs ip=dhcp

    Thanks

  • Hello,

    Rajnikant Jachak said:
    console=ttyO0,115200n8 rootwait rw mem=256M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti814xfb.v
    ram=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=10.1.1.243:/opt/targetfs ip=dhcp

    What are you using DM814 or DM816?

    Rajnikant Jachak said:

    gst-launch  -v \
        omx_videomixer name=mix \
        ! omx_ctrl \
        ! omx_videosink sync=true \
        filesrc location=M2959_1_ENG_3_5.png \
        ! pngdec ! ffmpegcolorspace  \
        ! imagefreeze \
        ! mix. \
        filesrc location=Dabang_4_1080p24_unscrambled_H264.mp4 ! qtdemux \
        ! queue ! h264parse ! omx_h264dec ! gstperf print-arm-load=1 ! omx_scaler \
        ! ffmpegcolorspace \
        ! mix.

    --------------------------------- ERROR ------------------------------------

    (gst-launch-0.10:1555): GLib-GObject-WARNING **: invalid cast from `GstBuffer' to `GstOmxBufferTransport'
    Caught SIGSEGV accessing address (nil)
    perf0: frames: 15       current: 6.06    average: 6.06  arm-load: 11
    Spinning.  Please run 'gdb gst-launch 1555' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.

    In this case, the using of ffmpegcolorspace component leads to this error in yours pipeline.

    I will continue to investigate.

    Best Regards,

    Margarita

  • Thanks Margarita for continued attention.

    I'm using DM1848 EVM and EZSDK version 5_05_02_00.

    Thanks

  • Hello Rajnikant Jachak,

    You could use videomixer element:

    gst-launch  --gst-debug=3  videomixer name=mix ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60  ! omx_videosink sync=true     filesrc location=12664924405.png   ! pngdec ! queue !  ffmpegcolorspace   ! imagefreeze !  mix.

    Is it working for you?

    Let me know the result.

    Best Regards,

    Margarita

  • Hello Margarita,

    I had tried videomixer element with following pipeline:

    gst-launch  -v \
        videomixer name=mix sink_1::xpos=520 sink_1::ypos=960 sink_1::alpha=0.3 sink_1::zorder=3 sink_2::xpos=400 sink_2::ypos=100 sink_2::zorder=2 \
        ! omx_ctrl display-device=HDMI \
        ! omx_videosink display-device=HDMI sync=true \
        filesrc location=M2959_1_ENG_3_5.png \
        ! pngdec ! queue ! ffmpegcolorspace \
        ! imagefreeze \
        ! mix. \
        filesrc location=Dabang_4_1080p24_unscrambled_H264.mp4 ! qtdemux \
        ! h264parse ! omx_h264dec ! queue ! gstperf print-arm-load=1 ! omx_scaler \
        ! ffmpegcolorspace \
        ! mix.

    ----------------- gstperf stats ---------------------------

    perf0: frames: 16       current: 15.99   average: 15.99 arm-load: 20
    perf0: frames: 20       current: 3.73    average: 9.65  arm-load: 100
    perf0: frames: 24       current: 3.89    average: 7.74  arm-load: 99
    perf0: frames: 28       current: 3.85    average: 6.76  arm-load: 100

    This pipeline achieves image overlay on video. But as you can see in gstperf statistics, the framerate drops drastically for videomixer on EVM (Original is 24 FPS).

    I moved to omx_videomixer as I think omx uses hardware acceleration to speed up the processing.

  • Hello Rajnikant Jachak,

    The frame rate dropped not because of using on omx_videomixer or videomixer element, it is dropped because of ffmpegcolorspace elements in the pipeline.

    ffmpegcolorspace — converts video from one colorspace to another.

    I will continue to investigate.

    Best Regards,

    Margarita