Other Parts Discussed in Thread: TVP7002
Hi,
(1) If the fps is not what I care about, how many channels of 1080P raw data capture is supported by one DM8168 at the same time? It seems this depends on VPSS capture ports? I want to use a DM8168 to capture as many as possible channels of 1080P raw data.
(2) How many 1080P channels of raw video data can be encoded by a DM8168 at the same time? Some docs say it can encode 3 channels of 1080P raw data at 60fps, is it true? If yes, does this mean it can also encode 6 channels of 1080P raw data at 30 fps? BTW: I am not care about D1.
(3) How many 1080P channels of H264 encoded bit stream can be decoded by a DM8168 at the same time?
(4) I want to connect as many as possible TVs using one DM8168 (HDMI, component, or DVO or VGA is OK for me), and each TV displays different contents, could you tell me the maximum number of TVs can be connected with one DM8168?
(5) I am considering to construct multiple DM8168s on a PCB board, to enhance the capabilities of one DM8168, what kind of interconnection can be used? For now, I just know such as network, are there some other ways to communicate between multiple DM8168s? Are there some demo boards on this?
Thanks in advance