I found some older postings here in TIe2e that DMA for SPI will be supported in future.
Is this running now ?
Does anybody use omap2_mcspi with DMA on DM8168 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I found some older postings here in TIe2e that DMA for SPI will be supported in future.
Is this running now ?
Does anybody use omap2_mcspi with DMA on DM8168 ?
Hi,
We have a patch on DM814x platform for the feature which is only for mcspi0:0.
It is never tested on DM816x and is only provided as reference. It is not officially supported by in linux PSP.
diff -Naur kernel_original/arch/arm/mach-omap2/devices.c kernel/arch/arm/mach-omap2/devices.c
--- kernel_original/arch/arm/mach-omap2/devices.c 2012-08-17 04:52:55.639082398 +0800
+++ kernel/arch/arm/mach-omap2/devices.c 2012-08-17 23:29:14.405074857 +0800
@@ -452,6 +452,18 @@
.end = OMAP2_MCSPI1_BASE + 0xff,
.flags = IORESOURCE_MEM,
},
+ {
+ //SPI0XEVT0: SPI0 Transmit 0
+ .start = 16,
+ .end = 16,
+ .flags = IORESOURCE_DMA,
+ },
+ {
+ //SPI0REVT0: SPI0 Receive 0
+ .start = 17,
+ .end = 17,
+ .flags = IORESOURCE_DMA,
+ },
};
static struct platform_device omap2_mcspi1 = {
diff -Naur kernel_original/drivers/spi/omap2_mcspi.c kernel/drivers/spi/omap2_mcspi.c
--- kernel_original/drivers/spi/omap2_mcspi.c 2012-08-17 04:53:15.931080125 +0800
+++ kernel/drivers/spi/omap2_mcspi.c 2012-08-17 23:41:39.433071468 +0800
@@ -40,8 +40,16 @@
#include <plat/clock.h>
#include <plat/mcspi.h>
#include <asm/mach-types.h>
+#include <asm/hardware/edma.h>
#define OMAP2_MCSPI_MAX_FREQ 48000000
+#define DUMMY_SLOTS 5
+
+#define STATIC_SHIFT 3
+#define TCINTEN_SHIFT 20
+#define ITCINTEN_SHIFT 21
+#define TCCHEN_SHIFT 22
+#define ITCCHEN_SHIFT 23
/* OMAP2 has 3 SPI controllers, while OMAP3 has 4 */
#define OMAP2_MCSPI_MAX_CTRL 4
@@ -99,10 +107,13 @@
#define OMAP2_MCSPI_WAKEUPENABLE_WKEN BIT(0)
+#define USE_DMA 1
+
/* We have 2 DMA channels per CS, one for RX and one for TX */
struct omap2_mcspi_dma {
int dma_tx_channel;
int dma_rx_channel;
+ enum dma_event_q eventq;
int dma_tx_sync_dev;
int dma_rx_sync_dev;
@@ -314,9 +325,14 @@
return 0;
}
+#define OMAP_DMA_DATA_TYPE_S8 0x01
+#define OMAP_DMA_DATA_TYPE_S16 0x02
+#define OMAP_DMA_DATA_TYPE_S32 0x04
+
static unsigned
omap2_mcspi_txrx_dma(struct spi_device *spi, struct spi_transfer *xfer)
{
+
struct omap2_mcspi *mcspi;
struct omap2_mcspi_cs *cs = spi->controller_state;
struct omap2_mcspi_dma *mcspi_dma;
@@ -325,9 +341,12 @@
int word_len, data_type, element_count;
int elements = 0;
u32 l;
- u8 * rx;
- const u8 * tx;
+ u8 *rx;
+ const u8 *tx;
void __iomem *chstat_reg;
+ struct edmacc_param param_set;
+ int temp_count;
+ u8 *tmp_buf;
mcspi = spi_master_get_devdata(spi->master);
mcspi_dma = &mcspi->dma_channels[spi->chip_select];
@@ -356,54 +375,86 @@
element_count = count >> 2;
}
+ /*
+ if tx!=NULL, then it means there is data to transfer
+ if tx==NULL, then ti means there is no data to transfer, but we still need send dummy data to generate clock for rx,
+ */
if (tx != NULL) {
- omap_set_dma_transfer_params(mcspi_dma->dma_tx_channel,
- data_type, element_count, 1,
- OMAP_DMA_SYNC_ELEMENT,
- mcspi_dma->dma_tx_sync_dev, 0);
-
- omap_set_dma_dest_params(mcspi_dma->dma_tx_channel, 0,
- OMAP_DMA_AMODE_CONSTANT,
- tx_reg, 0, 0);
-
- omap_set_dma_src_params(mcspi_dma->dma_tx_channel, 0,
- OMAP_DMA_AMODE_POST_INC,
- xfer->tx_dma, 0, 0);
+ xfer->tx_dma = dma_map_single(&spi->dev, (void *)xfer->tx_buf, element_count, DMA_TO_DEVICE);
+ if (dma_mapping_error(&spi->dev, xfer->tx_dma))
+ {
+ printk(KERN_INFO, "Sheng: Unable to DMA map a %d bytes"
+ " TX buffer\n", element_count);
+ return -ENOMEM;
+ }
+ temp_count = element_count;
+ }
+ else {
+
+ tmp_buf = (u8 *)kzalloc(element_count + 1, GFP_KERNEL);
+
+ xfer->tx_dma = dma_map_single(&spi->dev,(void *)tmp_buf, element_count + 1, DMA_TO_DEVICE);
+ if (dma_mapping_error(&spi->dev, xfer->tx_dma)) {
+ dev_dbg(KERN_INFO, "Sheng: Unable to DMA map a %d bytes"
+ " TX tmp buffer\n", element_count + 1 );
+ return -ENOMEM;
+ }
+ temp_count = element_count + 1;
}
+ //configuration of tx edma channel
+ if (tx != NULL || rx != NULL) {
+ edma_set_src(mcspi_dma->dma_tx_channel, xfer->tx_dma, INCR, W8BIT);
+ edma_set_dest(mcspi_dma->dma_tx_channel, tx_reg, INCR, W8BIT);
+ edma_set_src_index(mcspi_dma->dma_tx_channel, data_type, 0);
+ edma_set_dest_index(mcspi_dma->dma_tx_channel, 0, 0);
+ edma_set_transfer_params(mcspi_dma->dma_tx_channel, data_type, temp_count, 1, 0, ASYNC);
+
+ edma_read_slot(mcspi_dma->dma_tx_channel, ¶m_set);
+ param_set.opt |= (1 << TCINTEN_SHIFT);
+#define EDMA3CC_OPT(n) (0x4000 + 0x0 + (0x20 * n))
+ param_set.link_bcntrld = EDMA3CC_OPT(DUMMY_SLOTS);
+ param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(mcspi_dma->dma_tx_channel));
+ edma_write_slot(mcspi_dma->dma_tx_channel, ¶m_set);
+ }
+ //configuration of rx edma channel
if (rx != NULL) {
- elements = element_count - 1;
+ elements = element_count;
if (l & OMAP2_MCSPI_CHCONF_TURBO)
elements--;
+ xfer->rx_dma = dma_map_single(&spi->dev, (void *)xfer->rx_buf, elements, DMA_FROM_DEVICE);
+ if (dma_mapping_error(&spi->dev, xfer->rx_dma)) {
+ dev_dbg(KERN_INFO, "Sheng: Couldn't DMA map a %d bytes RX buffer\n", elements);
+ if (xfer->tx_buf != NULL)
+ dma_unmap_single(NULL, xfer->tx_dma, elements, DMA_TO_DEVICE);
+ return -ENOMEM;
+ }
- omap_set_dma_transfer_params(mcspi_dma->dma_rx_channel,
- data_type, elements, 1,
- OMAP_DMA_SYNC_ELEMENT,
- mcspi_dma->dma_rx_sync_dev, 1);
-
- omap_set_dma_src_params(mcspi_dma->dma_rx_channel, 0,
- OMAP_DMA_AMODE_CONSTANT,
- rx_reg, 0, 0);
-
- omap_set_dma_dest_params(mcspi_dma->dma_rx_channel, 0,
- OMAP_DMA_AMODE_POST_INC,
- xfer->rx_dma, 0, 0);
+ edma_set_src(mcspi_dma->dma_rx_channel, rx_reg, INCR, W8BIT);
+ edma_set_dest(mcspi_dma->dma_rx_channel,xfer->rx_dma, INCR, W8BIT);
+ edma_set_src_index(mcspi_dma->dma_rx_channel, 0, 0);
+ edma_set_dest_index(mcspi_dma->dma_rx_channel,data_type, 0);
+ edma_set_transfer_params(mcspi_dma->dma_rx_channel, data_type, elements, 1, 0, ASYNC);
+
+ edma_read_slot(mcspi_dma->dma_rx_channel, ¶m_set);
+ param_set.opt |= (1 << TCINTEN_SHIFT);
+ param_set.opt |= EDMA_TCC(EDMA_CHAN_SLOT(mcspi_dma->dma_rx_channel));
+ edma_write_slot(mcspi_dma->dma_rx_channel, ¶m_set);
}
-
- if (tx != NULL) {
- omap_start_dma(mcspi_dma->dma_tx_channel);
+ if (tx != NULL || rx != NULL) {
+ edma_start(mcspi_dma->dma_tx_channel);
omap2_mcspi_set_dma_req(spi, 0, 1);
}
if (rx != NULL) {
- omap_start_dma(mcspi_dma->dma_rx_channel);
+ edma_start(mcspi_dma->dma_rx_channel);
omap2_mcspi_set_dma_req(spi, 1, 1);
}
- if (tx != NULL) {
+ if (tx != NULL || rx != NULL) {
wait_for_completion(&mcspi_dma->dma_tx_completion);
- dma_unmap_single(NULL, xfer->tx_dma, count, DMA_TO_DEVICE);
-
+ dma_unmap_single(NULL, xfer->tx_dma, temp_count, DMA_TO_DEVICE);
+
/* for TX_ONLY mode, be sure all words have shifted out */
if (rx == NULL) {
if (mcspi_wait_for_reg_bit(chstat_reg,
@@ -417,51 +468,8 @@
if (rx != NULL) {
wait_for_completion(&mcspi_dma->dma_rx_completion);
- dma_unmap_single(NULL, xfer->rx_dma, count, DMA_FROM_DEVICE);
- omap2_mcspi_set_enable(spi, 0);
-
- if (l & OMAP2_MCSPI_CHCONF_TURBO) {
-
- if (likely(mcspi_read_cs_reg(spi, OMAP2_MCSPI_CHSTAT0)
- & OMAP2_MCSPI_CHSTAT_RXS)) {
- u32 w;
-
- w = mcspi_read_cs_reg(spi, OMAP2_MCSPI_RX0);
- if (word_len <= 8)
- ((u8 *)xfer->rx_buf)[elements++] = w;
- else if (word_len <= 16)
- ((u16 *)xfer->rx_buf)[elements++] = w;
- else /* word_len <= 32 */
- ((u32 *)xfer->rx_buf)[elements++] = w;
- } else {
- dev_err(&spi->dev,
- "DMA RX penultimate word empty");
- count -= (word_len <= 8) ? 2 :
- (word_len <= 16) ? 4 :
- /* word_len <= 32 */ 8;
- omap2_mcspi_set_enable(spi, 1);
- return count;
- }
- }
-
- if (likely(mcspi_read_cs_reg(spi, OMAP2_MCSPI_CHSTAT0)
- & OMAP2_MCSPI_CHSTAT_RXS)) {
- u32 w;
-
- w = mcspi_read_cs_reg(spi, OMAP2_MCSPI_RX0);
- if (word_len <= 8)
- ((u8 *)xfer->rx_buf)[elements] = w;
- else if (word_len <= 16)
- ((u16 *)xfer->rx_buf)[elements] = w;
- else /* word_len <= 32 */
- ((u32 *)xfer->rx_buf)[elements] = w;
- } else {
- dev_err(&spi->dev, "DMA RX last word empty");
- count -= (word_len <= 8) ? 1 :
- (word_len <= 16) ? 2 :
- /* word_len <= 32 */ 4;
- }
- omap2_mcspi_set_enable(spi, 1);
+ dma_unmap_single(NULL, xfer->rx_dma, elements, DMA_FROM_DEVICE);
+ kfree((void *)tmp_buf);
}
return count;
}
@@ -469,6 +477,7 @@
static unsigned
omap2_mcspi_txrx_pio(struct spi_device *spi, struct spi_transfer *xfer)
{
+
struct omap2_mcspi *mcspi;
struct omap2_mcspi_cs *cs = spi->controller_state;
unsigned int count, c;
@@ -536,8 +545,7 @@
}
*rx++ = __raw_readl(rx_reg);
- dev_vdbg(&spi->dev, "read-%d %02x\n",
- word_len, *(rx - 1));
+ dev_vdbg(&spi->dev, "read-%d %02x\n", word_len, *(rx - 1));
}
} while (c);
} else if (word_len <= 16) {
@@ -660,6 +668,7 @@
static int omap2_mcspi_setup_transfer(struct spi_device *spi,
struct spi_transfer *t)
{
+
struct omap2_mcspi_cs *cs = spi->controller_state;
struct omap2_mcspi *mcspi;
struct spi_master *spi_cntrl;
@@ -700,7 +709,6 @@
l &= ~(OMAP2_MCSPI_CHCONF_IS|OMAP2_MCSPI_CHCONF_DPE1);
l |= OMAP2_MCSPI_CHCONF_DPE0;
}
-
/* wordlength */
l &= ~OMAP2_MCSPI_CHCONF_WL_MASK;
l |= (word_len - 1) << 7;
@@ -737,6 +745,7 @@
static void omap2_mcspi_dma_rx_callback(int lch, u16 ch_status, void *data)
{
+
struct spi_device *spi = data;
struct omap2_mcspi *mcspi;
struct omap2_mcspi_dma *mcspi_dma;
@@ -744,14 +753,17 @@
mcspi = spi_master_get_devdata(spi->master);
mcspi_dma = &(mcspi->dma_channels[spi->chip_select]);
- complete(&mcspi_dma->dma_rx_completion);
-
/* We must disable the DMA RX request */
omap2_mcspi_set_dma_req(spi, 1, 0);
+
+ complete(&mcspi_dma->dma_rx_completion);
+
+
}
static void omap2_mcspi_dma_tx_callback(int lch, u16 ch_status, void *data)
{
+
struct spi_device *spi = data;
struct omap2_mcspi *mcspi;
struct omap2_mcspi_dma *mcspi_dma;
@@ -759,10 +771,10 @@
mcspi = spi_master_get_devdata(spi->master);
mcspi_dma = &(mcspi->dma_channels[spi->chip_select]);
- complete(&mcspi_dma->dma_tx_completion);
-
/* We must disable the DMA TX request */
omap2_mcspi_set_dma_req(spi, 0, 0);
+
+ complete(&mcspi_dma->dma_tx_completion);
}
static int omap2_mcspi_request_dma(struct spi_device *spi)
@@ -770,25 +782,43 @@
struct spi_master *master = spi->master;
struct omap2_mcspi *mcspi;
struct omap2_mcspi_dma *mcspi_dma;
+ struct edmacc_param dummyPaRAMSet;
+ int r;
mcspi = spi_master_get_devdata(master);
mcspi_dma = mcspi->dma_channels + spi->chip_select;
-
- if (omap_request_dma(mcspi_dma->dma_rx_sync_dev, "McSPI RX",
- omap2_mcspi_dma_rx_callback, spi,
- &mcspi_dma->dma_rx_channel)) {
+
+ r = edma_alloc_channel(mcspi_dma->dma_rx_sync_dev, omap2_mcspi_dma_rx_callback, spi, 0);
+ if (r < 0) {
dev_err(&spi->dev, "no RX DMA channel for McSPI\n");
return -EAGAIN;
}
-
- if (omap_request_dma(mcspi_dma->dma_tx_sync_dev, "McSPI TX",
- omap2_mcspi_dma_tx_callback, spi,
- &mcspi_dma->dma_tx_channel)) {
- omap_free_dma(mcspi_dma->dma_rx_channel);
- mcspi_dma->dma_rx_channel = -1;
+ mcspi_dma->dma_rx_channel = r;
+
+ r = edma_alloc_channel(mcspi_dma->dma_tx_sync_dev, omap2_mcspi_dma_tx_callback, spi, 0);
+ if (r < 0) {
dev_err(&spi->dev, "no TX DMA channel for McSPI\n");
return -EAGAIN;
}
+ mcspi_dma->dma_tx_channel = r;
+
+ /*setting up dummy slots to prevent tx EVENT MISSED ERROR
+ here using fixed DUMMY_SLOTS, better method is to automatically allocate unused channel
+ */
+
+ edma_read_slot(DUMMY_SLOTS, &dummyPaRAMSet);
+
+ dummyPaRAMSet.opt = 0x00000000;
+ dummyPaRAMSet.src = 0x00000000;
+ dummyPaRAMSet.a_b_cnt = 0x00000001;
+ dummyPaRAMSet.dst = 0x00000000;
+ dummyPaRAMSet.src_dst_bidx = 0x00000000;
+ dummyPaRAMSet.link_bcntrld = 0x0000ffff;
+ dummyPaRAMSet.src_dst_cidx = 0x00000000;
+ dummyPaRAMSet.ccnt = 0x00000000;
+
+ edma_write_slot(DUMMY_SLOTS, &dummyPaRAMSet);
+ edma_link(mcspi_dma->dma_tx_channel,DUMMY_SLOTS);
init_completion(&mcspi_dma->dma_rx_completion);
init_completion(&mcspi_dma->dma_tx_completion);
@@ -828,10 +858,8 @@
if (mcspi_dma->dma_rx_channel == -1
|| mcspi_dma->dma_tx_channel == -1) {
/* TI81XX has EDMA and not SDMA, hence overriding SDMA usage */
- if (!cpu_is_ti81xx())
- ret = omap2_mcspi_request_dma(spi);
- else
- ret = 0;
+ /* Sheng: using edma here for TI81XX*/
+ ret = omap2_mcspi_request_dma(spi);
if (ret < 0)
return ret;
}
@@ -865,11 +893,11 @@
mcspi_dma = &mcspi->dma_channels[spi->chip_select];
if (mcspi_dma->dma_rx_channel != -1) {
- omap_free_dma(mcspi_dma->dma_rx_channel);
+ edma_free_channel(mcspi_dma->dma_rx_channel);
mcspi_dma->dma_rx_channel = -1;
}
if (mcspi_dma->dma_tx_channel != -1) {
- omap_free_dma(mcspi_dma->dma_tx_channel);
+ edma_free_channel(mcspi_dma->dma_tx_channel);
mcspi_dma->dma_tx_channel = -1;
}
}
@@ -901,6 +929,7 @@
int par_override = 0;
int status = 0;
u32 chconf;
+ int i;
m = container_of(mcspi->msg_queue.next, struct spi_message,
queue);
@@ -948,27 +977,25 @@
}
mcspi_write_chconf0(spi, chconf);
-
if (t->len) {
unsigned count;
- /* RX_ONLY mode needs dummy data in TX reg */
- if (t->tx_buf == NULL)
- __raw_writel(0, cs->base
- + OMAP2_MCSPI_TX0);
-
- if (m->is_dma_mapped || t->len >= DMA_MIN_BYTES)
+ //m->is_dma_mapped = 1;
+ if (USE_DMA || (m->is_dma_mapped || t->len >= DMA_MIN_BYTES))
count = omap2_mcspi_txrx_dma(spi, t);
else
+ {
+ /* RX_ONLY mode needs dummy data in TX reg */
+ if (t->tx_buf == NULL)
+ __raw_writel(0, cs->base + OMAP2_MCSPI_TX0);
count = omap2_mcspi_txrx_pio(spi, t);
+ }
m->actual_length += count;
-
if (count != t->len) {
status = -EIO;
break;
}
}
-
if (t->delay_usecs)
udelay(t->delay_usecs);
@@ -1038,8 +1065,7 @@
OMAP2_MCSPI_MAX_FREQ/(1<<16));
return -EINVAL;
}
-
- if (m->is_dma_mapped || len < DMA_MIN_BYTES)
+ if ( m->is_dma_mapped || len < DMA_MIN_BYTES)
continue;
/* Do DMA mapping "early" for better error reporting and
@@ -1048,8 +1074,7 @@
* for previous transfers on *ALL* exits of this loop...
*/
if (tx_buf != NULL) {
- t->tx_dma = dma_map_single(&spi->dev, (void *) tx_buf,
- len, DMA_TO_DEVICE);
+ t->tx_dma = dma_map_single(&spi->dev, (void *) tx_buf, len, DMA_TO_DEVICE);
if (dma_mapping_error(&spi->dev, t->tx_dma)) {
dev_dbg(&spi->dev, "dma %cX %d bytes error\n",
'T', len);
@@ -1060,11 +1085,9 @@
t->rx_dma = dma_map_single(&spi->dev, rx_buf, t->len,
DMA_FROM_DEVICE);
if (dma_mapping_error(&spi->dev, t->rx_dma)) {
- dev_dbg(&spi->dev, "dma %cX %d bytes error\n",
- 'R', len);
+ dev_dbg(&spi->dev, "dma %cX %d bytes error\n",'R', len);
if (tx_buf != NULL)
- dma_unmap_single(NULL, t->tx_dma,
- len, DMA_TO_DEVICE);
+ dma_unmap_single(NULL, t->tx_dma, len, DMA_TO_DEVICE);
return -EINVAL;
}
}
@@ -1258,18 +1281,29 @@
goto err2;
}
- mcspi->dma_channels = kcalloc(master->num_chipselect,
- sizeof(struct omap2_mcspi_dma),
- GFP_KERNEL);
+ mcspi->dma_channels = kzalloc(master->num_chipselect*sizeof(struct omap2_mcspi_dma), GFP_KERNEL);
if (mcspi->dma_channels == NULL)
goto err3;
for (i = 0; i < num_chipselect; i++) {
- mcspi->dma_channels[i].dma_rx_channel = -1;
- mcspi->dma_channels[i].dma_rx_sync_dev = rxdma_id[i];
+ r = platform_get_resource(pdev, IORESOURCE_DMA, 0);
+ if (r == NULL) {
+ status = -ENODEV;
+ goto err1;
+ }
+ mcspi->dma_channels[i].dma_tx_sync_dev = r->start;
mcspi->dma_channels[i].dma_tx_channel = -1;
- mcspi->dma_channels[i].dma_tx_sync_dev = txdma_id[i];
+ //printk(KERN_INFO"allocated tx channel:%d\n",r->start);
+
+ r = platform_get_resource(pdev, IORESOURCE_DMA, 1);
+ if (r == NULL) {
+ status = -ENODEV;
+ goto err1;
+ }
+ //printk(KERN_INFO"allocated rx channel:%d\n",r->start);
+ mcspi->dma_channels[i].dma_rx_sync_dev = r->start;
+ mcspi->dma_channels[i].dma_rx_channel = -1;
}
if (omap2_mcspi_reset(mcspi) < 0)
You can find the EDMA event number from data maunnal(SPRS614D) Table 8-34. EDMA Default Synchronization Events
Best Regards,
Eason
Thanks for the patch, I will try to add it into our omap2_mcspi.
Our goal is the improvent of SPI.
We use 16 MHz SPI clock and want to transmit and receive 320 Bytes every millisecond in duplex via SPI.
This is possible but we want to decrease the load for DM8168.
I also found that TURBO mode is an option to became faster, but this is only for receive.
We use SPI in duplex mode und must improve transmit and receive speed at the same time.
One idea was to use FIFO and share the 64 byte FIFO buffer for transmit and receive but I could not find a proper
example for this. Do You have any experience with using the FIFO mode for SPI ?
Ok, I have got EDMA working in omap2_mcspi on DM8168. We got some speed improvment.
Next step will be to add the FIFO buffer.
Thanks for the patch!
Best regards
After enabling EDMA for omap2_mcspi we try to setup FIFO mode for duplex.
I am not sure how to use FIFO with shared buffer 32 / 32 Byte for transmit / receive at the same time.
Does anybody have experinece with this problem ?