Our DM8168 design can't totally pass the eye diagram test even though we have populated the 44.2 ohm at pin USB0_R1 and USB1_R1. The eye opening is marginal to eye mask. This small eye opening cause specific USB device is unstable. After changing USB0_R1 and USB1_R1 to 33 ohm, the issue is resolved and the eye opening looks good. I am not sure if there is any side effect after change this resistor 33 ohm. someone can comment it ?
Our USB trace length is less than 1800 mil, the impedance is 90 ohm. Full GND plane for return path. No stub.