Hi,
Is it possible to capture two simultaneous 1920 x 1200 @ 50 fps video using single DM8168 processor?
Regards,
Siddharth
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to capture two simultaneous 1920 x 1200 @ 50 fps video using single DM8168 processor?
Regards,
Siddharth
Hi Siddharth,
DM8168 HDVPSS (HD Video Processing Subsystem) can capture two simultaneous ( up to HD resolution, 1920x1080@60) video channels.
For more details see the below pointers:
1. DM816x datasheet
HD Video Processing Subsystem (HDVPSS)
– Two 165-MHz HD Video Capture Channels
• One 16-Bit or 24-Bit and One 16-Bit Channel
• Each Channel Splittable Into Dual 8-Bit Capture Channels
1 16-bit and 24-bit HD Capture Channel or 2 8-bit SD Capture Channels AND 1 16-bit HD Capture Channel or 2 8-bit SD Capture Channels
Two (one 16-bit, 24-bit and one 16-bit) independently configurable external video input capture ports (up to 165 MHz).
– 16-bit and 24-bit HD digital video input or dual clock independent 8-bit SD inputs on each capture port.
• VIN[0] can accept single-channel 16-bit, 24-bit (YCbCr and RGB) video or dual-channel 8-bit (YCbCr) video.
• VIN[1] can accept single-channel 16-bit (YCbCr) video or dual-channel 8-bit (YCbCr) video.
2. DM816x TRM, section 2.1.5.6 Video Capture Features
Regards,
Pavel
Hi Pavel
Thank you for your inputs. We did gone through the datasheets and TRMs to find out support for two 1920 x 1200 @ 50 fps video captures. From theoretical calculations, it seems that it is possible to capture two such videos. But, I posted this query here hoping that if anybody from community has already done anything similar to that, I can learn from his/her experiences and correct the architecture of our product if needed.
Regards
Siddharth
Yes, it is possible, we were capturing 2 channels of 1080p@60fps, so 50fps is also possible.
Rgds,
Brijesh