Part Number: TMS320DM8148
Tool/software: Linux
I Have seen the sample application for edma ,which can only be accessed from kernel space , How Can i use EDMA in my application . And How can we change the maximum size for Transfer.?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320DM8148
Tool/software: Linux
I Have seen the sample application for edma ,which can only be accessed from kernel space , How Can i use EDMA in my application . And How can we change the maximum size for Transfer.?
Ammar said:And How can we change the maximum size for Transfer.?
The EDMA transfer size is configured through ACNT, BCNT and CCNT params. Refer to DM814x TRM for more details.
There is also DBS (Default Burst Size) which is also configurable, see below e2e thread: