This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uPP start signal and EOL interrupt behavior in the muti-line receive mode?

I understand you can disable START signal and use byte counts per line to figure out when to start a next line, however, it was not clear if uPP receiver will honor the START signal and ignore the byte counts in the DMA when the START signal is asserted before the current line reach expected byte counts?

I have two questions in this scenario where I set up multi-line window with byte counts = line offset = N:

1. Would the uPP receive multiple lines with different sizes (but not exceeding N bytes) correctly using to the START signal?

2. If yes, would the end of line interrupt fire as a new line starts even though previous line was smaller than N bytes?

 

I'd appreciate your help!