Hi
I'd like to confirm a DDR Drive Strength for mDDR supported.
I' can't understand the decryption of DDRDRIVE in L138 TRM.
http://www.ti.com/litv/pdf/spruh77a
In Spruh77a.pdf, DDRDRIVE0 is described below:
0 For DDR2, normal drive strength. For mobile DDR, full drive strength.
1h For DDR2, weak drive strength. For mobile DDR, 1/2 drive strength.
2h For DDR2, reserved. For mobile DDR, 1/4 drive strength.
3h For DDR2, reserved. For mobile DDR, 3/4 drive strength.
However, In JESD209B, Drive strength is described below:
A6 A5 Drive Strength
0 0 Full Strength Driver
0 1 Half Strength Driver
1 0 Optional Quarter Strength Driver
1 1 Optional Octant Strength Driver
Where does this difference come from?
I think L138 TRM is wrong. If DDRDRIVE0[1:0] is 3h, It should be configured 1/8 with mDDR.
#In case of AM335x, when Drive strength is 3h, It means to set 1/8 with mDDR.
Best Regards
Takao