Other Parts Discussed in Thread: OMAP-L138
Hi All,
(On the c6000 core, not the ARM)
We are attempting to Synchronize the eCAP0-eCAP2 counter (TSCTR) on start up using the SWSYNC from eCAP0. All of the eCAPs are configured as follows:
- All eCAPs in CAPMODE
- All are in ONE SHOT mode
- On eCAP0 (Master for syncing)
- SYNCI_EN is 0 (DISABLE)
- SYNCO_SEL is 0 (SYNCIN)
- On eCAP1
- SYNCI_EN is 1 (ENABLE)
- SYNCO_SEL is 0 (SYNCIN)
- On eCAP2
- SYNCI_EN is 1 (ENABLE)
- SYNCO_SEL is 2 (DISABLE)
Once finished, we set SWSYNC to 1 on the eCAP0 to sync all eCAPs. However, none of the capture port TSCTR registers reflect the value of their corresponding shadow register CTRPHS. We were wondering if there is a caveat on using the SWSYNC (instead of the PWM Pulse) to sync that we are missing.
Thank you,
Arya B.