Other Parts Discussed in Thread: OMAPL138
HI
I am using OMAPL138 LCDK I am trying to use a Logitech HD web Cam to capture video and display through VGA port to the LCD when i connected it after booting the SD card on teraterm after logging in the device shows which like this
omapl138-lcdk login: root
root@omapl138-lcdk:~# usb 1-1: USB disconnect, device number 2
usb 1-1: new full speed USB device number 3 using ohci
usb 1-1: New USB device found, idVendor=046d, idProduct=0825
usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=2
usb 1-1: SerialNumber: C1D14B60
after it it again comes to the promt how can i interface the USB web cam to this kit pls help..
i want to use the usb web cam with the opencv library for some image processing so kindly help for interfacing of USB camera with the OMAP L138LCDK an how to use the OPENCV on this kit. pls help it is necessary for my project