Other Parts Discussed in Thread: TXB0108, TVP5147
I'm trying to connect my custom made camera board to the camera connector of the LCDK board. However I observed from the schematic that port CVIDEO_DIN0-7 is shared with the digital video decoder TVP5147. How can I disable this chip without board modification? What is the purpose of r pull-up (R244 - R251)? Finally with R244 - R251 populate will the pull up resistor confuse the logic converter I use (TXB0108)? I need to use it because the LCDK board use 3.3v I/O but my camera module use 1.8v I/O.
Regards,
Palm