Other Parts Discussed in Thread: OMAP-L137, BIOSLINUXMCSDK, OMAPL138
The products being developed using the OMAP-L137 to the following error:
Loading from NAND 512MiB 3,3V 8-bit, offset 0xc0000
Image Name: Linux-2.6.18_pro500-da830_omapl1
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1673452 Bytes = 1.6 MB
Load Address: c0008000
Entry Point: c0008000
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.18_pro500-da830_omapl1
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1673452 Bytes = 1.6 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
This problem does not happen often, it appears once every few months.
While searching a solution, I found a post with a similar issue in TI forum.
http://e2e.ti.com/support/embedded/linux/f/354/t/73788
The content of the post,Richard Counts wrote that there is a problem with the U-BOOT.
Processor and U-Boot is different. But the problem is similar.
I would like to know that there arn no problem in the U-BOOT code of OMAPL137.
I am using the code and hardware information is as follows.
OMAPL-137 custom board with a NAND FLASH(MT29F4G08ABADAWP).
The codes used were downloaded from the site below.
http://processors.wiki.ti.com/index.php/Installing_the_Software_for_OMAP-L137
REL_LSP_02_20_00_07.tgz(UBL, U-BOOT)
mvl_5_0_0_demo_lsp_setuplinux_02_20_00_07.bin(KERNEL)